Part Number: TAS5733L Tool/software: Linux Hi Shawn,
I implemented the volume table using the register 0x07 values. But we are facing one random issue.
when we play the song and increasing the gain after the -6db (-6 to 24db) we get the glitches spikes…
Part Number: TAS5733L Tool/software: Linux Hi,
I am using TAS5733l Amp, for implementing volume table when i try to write on 0x07 (master volume reg) register, which following
0x0000 24.000 0x0001 23.875 ... (0.125 dB steps) 0x03FE –103.750 0x03FF …
Part Number: TAS5733L Hi,
My customer would like to drive 4ohm speakers at 2x15W with a PVDD=16.5V continuous operation. The Output Power vs. PVDD graph does not specify data past 15V. Can you confirm this is ok across 4ohms?
Also, regarding heat management…
Part Number: TAS5751M-TAS5733L-SW Other Parts Discussed in Thread: TAS5733 , PCM2706 , TAS5713 , TAS5751M , TAS5733L On page 1 of the datasheets of both TAS5733 and TAS5751, it is claimed that the devices support 3-wire I2S (no MCLK needed), however there…
Part Number: TAS5733L One of my customers is attempting to get the TAS5733L running in one of their solutions.
Customer used the auto-generated files from the PurePath console to test out functionality, but is getting no output from the amp.
(1) Are there…
Part Number: TAS5733L Team,
TAS5733L datasheet states the below for PVDD:
"16.5 V is the maximum recommended voltage for continuous operation of the TAS5733L device. Testing and characterization of the device is performed up to and including 16.5…
Part Number: TAS5733LEVM Hi,
I have submitted the request for PPC3 TAS5733LEVM plug-in in your website yesterday, but I haven't received approval yet, so today I submitted again. In addition, our customer has submitted it as well. So, could you please…
Part Number: TAS5733L
Hi,
The TAS5733L is being considered in for a new design. The part drives up to 2 speakers at 10W. However, the design only has a single 10W speaker. The design uses an I2S audio output, so this is a requirement. This part seems…