Testing is on our system. The schematic of the TAS5755M section is below. The 3.3V supply is present as soon as system power is applied. Initialization sequence is: 1) negate PDN 2) wait 10 ms 3) enable PVDD (26V supply) 4) wait 10 ms 5) negate RESET 6…
Part Number: TAS5755M TAS5755 i n the PBTL mode, only B and D channels have output, but A and C channels have no output, and there was no VCC/2 level. This is very different from the specification. What is the reason for this problem? There is no problem…
Part Number: TAS5755MTAS5755M output PWM wave is ok, but no sound output. Could you provide I2C code? The input I2S signal is connected to the DAC, and the output sound is no problem.
Part Number: TAS5755M I'm using a TAS5755M in an application. I have it mostly working as required (2.1, BD mode, biquads used as active crossovers and bass/treble shelf filters). I'm trying to get DRC working but am finding a dearth of documentation…
Part Number: TAS5755M Dear TI group,
We use TAS5755M drive a Subwoofer with 3R@40W, and OUTPUT power=32W,Appendix show config and Schematic,
after work on a fewer miniute,TAS5755M occurs a error output state,OUTA&B=14V ,OUTC&D=0.4V。
What are the…
Part Number: TAS5755M Hi Ti Team,
Please help check the schematic of TAS5755. By the way, WHEN I was debugging TAS5755, I found that the bass part was very poor, please help to give some suggestions.