Hi Switch,
1. As said, TAS5755 does not support 1.1 mode because OUTA and OUTB is set as SE output and OUTC/OUTD is set as BTL output in 2.1 mode , you may hear nothing in TW channel.
2. We suggest to use GDE GUI to debug TAS5755, link is listed…
Part Number: TAS5755M Other Parts Discussed in Thread: TAS5711 , TAS5751M We have a number of products that use the TAS5755M Amplifier.
Currently we use the TAS5711 GDE to configure the register maps for the device.
However the TAS57X1 GDE isn't perfect…
Part Number: TAS5755M Other Parts Discussed in Thread: PCM5121 , Scenario: PCB with 2x TAS5755 and 1x PCM5121 supplied with MCLK(512xfs), BCLK, LRCLK and SDATA in I2S 24-bit 48khz.
I'm facing an issue with the TAS5755M when PVDD voltage is between around…
Part Number: TAS5755M Hello,
Our customer used TAS5755M with PBTL mode, when finished configuration, only C&D channel have output, there is no output on A&B channel, the speaker has voice but also has noise, in addition, the speaker is very hot. Below…
Part Number: TAS5755M
Hi team,
Regarding the PBTL mode setting of TAS5755M, the customer feedbacked that it is not necessary to set the register value in the following screenshot to work normally.
The customer's register values are as follows. How to…
Part Number: TAS5755M Other Parts Discussed in Thread: TAS5711 ,
Hello, engineers!
I am designing a 2.1 digital audio amplifier. By now I had used TAS5711/31 GDE to calculate the BQ4a coefficients. Now I need to calculate it on my own. I read the treads…
Part Number: TAS5755M Other Parts Discussed in Thread: DIR9001 hi,
I have designed a PCB for audio amplifier with TAS5755 and DIR9001 as an SPDIF input.
It is playing audio from a PC with TAS's default settings, now. It is time to set the equalizers…
Part Number: TAS5755M Hi,
I would like to interface I2S mic directly to TAS5755M and get 50W mono output. Please clarify if this is possible.
Awaiting your reply.
Thanks
Part Number: TAS5755M Is there ever going to be an update to the TAS57xx GDE?
As far as I can see the latest version is Version 2.1 Build 8 and is 13 years old!
It doesn't run too well on Windows 10, and doesn't fully support the TAS5755M :-(…
Part Number: TAS5755M Hi sir
we have above questions need your support,pls help check it,tks!
(1)Is the 0x39 register The length of the register generated by the UI interface is 8 But the manual says that 4 What is the effect of this write?
(2)There are…