Part Number: TAS5755M Hi sir
we use TAS5755M design as 2*20W+50W(2*4ohms+6ohms), however, we find Bass cannot be output 50W power and the THD is very weak , When using 6 ohms, a little gain is distorted only use 8 ohms can can be improved but the power can…
Part Number: TAS5755M Hi sir
This is the configuration of the tas software interface and the actual scan of the level curve. After the register is modified, the change of the bass curve does not change according to the value of the register, and the left…
Part Number: TAS5755M Hi, we apply the TAS5755 on an 2.1 speaker system, we measured the max. power output level vs distortion, but found the performance was different from the EVM board. Pls find below the initial data and the measuring data.
! I2C Configuration…
Part Number: TAS5755M Other Parts Discussed in Thread: TAS5731 Hi Team,
We are designing with TAS5755 and wanted to check if the following configuration would be possible. Would it be possible to use one of the mixer modules in the amplifier (I2C register…
Part Number: TAS5755M I wish to interface the TAS5755 to an audio streaming module. It is an off the shelf module from a world-class supplier.
The audio module runs in slave mode, so BCLK, LRCLK must be provided to it. It does not even have a connection…
Part Number: TAS5755M Other Parts Discussed in Thread: PCM5141 , DRV612 , PCM5121 , DRV604 I have a design based on TAS5755M Amp in a 2.0 BTL 50+50W configuration.
The client would like to add line-out to this device now too. Should I just multiplex the I2S…
Part Number: TAS5755M Dears:
When we use TAS5755M do PBTL Mode 24V/2ohm /50W and found it will shutdown when power reach 50W, Could you please help check the schematic ? Thanks .
Part Number: TAS5755M Hi we have planned to use TAS5755MDFD in one of our project.We have samples of TAS5755MDFD chip. where we found that VREG pin ( pin number 42) & AVDD pin( pin number 9) of TAS5755MDFD gets continuity when checked by multimeter…
Part Number: TAS5755M Hi,we use TAS5755 design as 2.1 module,however,when we write the code into TAS5755M,it cannot output voice and we find the SSTIMER pin is left floating,the code as attachment ,pls help check it and give some suggestions how to debug it,tks! tas5755_cfg…
Part Number: TAS5755M hi,
We have designed our custom board with TAS5755MDFD audio chip and interfaced it to Nvidia TX2 SOM ( where it runs with linux operating system in it ), but we can't able to drive audio signal to the speaker. We have bought a EVM…