Part Number: TAS5755M Other Parts Discussed in Thread: , TAS5731 Hi expert,
My customer is looking at TAS5755M process flow in the datasheet, but it is not clear on the location of volume components listed below.
0x07 Master volume 1 Description shown…
Part Number: TAS5755M hi,
We have designed our custom board with TAS5755MDFD audio chip and interfaced it to Nvidia TX2 SOM ( where it runs with linux operating system in it ), but we can't able to drive audio signal to the speaker. We have bought a EVM…
Part Number: TAS5755M Hi,
I have some question in using TAS5755M's.
In 2.1 application, the application Diagram as below:
when the application of the 2.1 mode is as follows,
is the output of the power amplifier OUT_A and OUT_B output positive…
Part Number: TAS5755M Other Parts Discussed in Thread: TAS5711 Hi,
I am use TAS5755M, I need TAS5755M drive. But there is no download point on the official website. Could TI provide TAS5755M's drive?
Thanks.
Part Number: TAS5755MTAS5755M Class D Audio Power Amplifier For sound speaker. The questions are as follows: The bass effect of TAS5755M power amplifier is not ideal, and the bass power can not always reach the maximum required by chip design. As a result…
Part Number: TAS5755M I have a PCB design (mine) that uses an Analog Devices SSM3582 with I2S input, the client wants me to replace this Amp with the TAS5755M so I bought the TAS5755M Evaluation PCB and have it running well from an analog input.
My PCB…
Part Number: TAS5755M Hi Sirs, Would you please advise the TAS5755M's Junction-to-Board Characterization Parameter as we marked in the picture below? Thank you and Best regards, Wayne Chen 02/21/2018
Other Parts Discussed in Thread: TAS5766MRMTEVM , TAS5766M Hi all,
we have a TAS5766DCA_REF1 daughter board on an PurePath-CMBEVM-CB RevD Motherboard. This combination works with the PurePath Console 1.16 but not with the latest Pure Path 3. There we have…
Part Number: TAS5755M
Hi,
Could you please tell me the adjustable minimum and maximum values for the DRC offset1 parameter ? It seems that the offset gain increases if setting 0dB ~ 12dB to DRC offset1 but the offset gain decreases if setting >12dB …
Part Number: TAS5755M Hi,
The output level after DRC1 is difference between the changing ch1_volume and the changing master_volume if using TAS5755MEVM with PBTL mode. So, what are the possible causes for this symptom ?
Best regards, Kato