Part Number: TAS5755M
HI Team, Customer is developing TAS5755 on the project. Can customer implement the following way for the I2S?
1. if the WCLK is 44.1KHz or 48KHz, TAS5755 will only adapt 3 wire I2S (BCLK, WCLK and DIN). the MCLK from internal PLL…
Shawn,
Some communication has taken place between myself and Adam S on this via email; part of that communication established that the TAS5755M does not have 2 bytes for master volume register, it has one. Are you checking my register settings against…
Part Number: TAS5755M Hi Sirs, According to the TAS5755 specification, the Rise/fall time for SCLK/LRCLK spec =MAX 8ns, customer's SOC's WS: Rise = 15.83 Fall = 14.08 SCK: Rise = 25.44ns Fall = 26.08ns which are over TAS5755's specifications. …
Gabriel,
The components window is representative of the actual device structure. You cannot rearrange the blocks as they are physically part of the IC. This is not reconfigurable like an FPGA or similar.
Regards,
-Adam
Part Number: TAS5755M
Hi Team, TAS5755 0x51 and 0x52 has three mixer each. The GUI can set the max value is 15.9.
Does this mean 15.9dB on each input? And this mixer can be used for gain increasing if volume is too small. is that right?
BR, SHH
Part Number: TAS5755M
Hi Team, Customer uses TAS5755 on 3 wire connection. However, the audio source send 32kHz WCLK 16bit I2S format.
Customer set 0x07 to 0xff or register 0x06 to 0x07 to mute the audio output, but fail.
Can you duplicate this case and…
Part Number: TAS5755M
Hi Team, Cusotmer uses TAS5755. the WCLK 48KHz can output notmal sound. If WCLK is 32KHz, the output sound is abnormal.
If cusotmer change WCLK to 32 KHz or 44.1KHz, any register value need to change?
BR, SHH
Part Number: TAS5755M Other Parts Discussed in Thread: TAS5711 hi
Q1:how is the power consumption at PDN low active(Reset high deactivated)? Datasheet do not show.
Q2:Is it the same when enter shutdown by setting register 0x05?
Q3:As for TAS5780,when I…
Part Number: TAS5755M I have heard the engineers who have used TAS5755, when the IIS signal is input, if the halfway signal is interrupted and re connected, there will be a murmurs, the problem of the output signal interruption, is this the case?
What…
Part Number: TAS5755M TAS5755 in 2.1 mode: When choosing 2.1 mode,How many watts can the maximum power be achieved?
working voltage:12v
TAS5755 in 2.1 mode: Can the following three audio output power be achieved? (speakers:12W,4Ω) 1 Group: 12W Audio…