Kawasaki-San,
Please use the GUI. The TAS5755M uses the TAS5731 GUI as linked on the TAS5755MEVM page.
Click on CH1_volume and on the right side you will see that register 0x08 is there. The same can be done for CH2_volume, sub_volume, and MASTER volume…
Part Number: TAS5755M This is a new design prototype for a Bluetooth Speaker project. I'm driving this Amp from a TLV320 that is configured for 16 bit I2S output and the project is a respin to introduce the TAS5755M as a replacement for an Analog Devices…
Part Number: TAS5755M
Hello
My customer intend to use 2.1ch for TAS5755M .
I had tested TAS5755MEVM by myself.
SSTIMER pin is as default ( 2.2nF is between SS timer and gnd)
In case 0x1A register is 1Ah ( SSTIMER enabled), POP is seen, 0x1A is 88h, no…
Part Number: TAS5755M The TAS5755MEVM.pdf document shows the diagram below where the non-driven side of a single ended (SE) output has SINGLE-ENDED SPLIT-CAPs and/or do-not-populate resistors in a potential divider. This is confusing because the data…