Part Number: TAS5756M Hello,
We are staring a project using TAS5756M, how can we get access for TAS5756m in pure-path 3?
My TI ID is: xuqm@hualu.com.cn
Best Regards
Castor
Part Number: TAS5756M Other Parts Discussed in Thread: TAS5754M , TLV320AIC3204 I'm undoubtedly overlooking something simple, but I cannot read GPIO for some reason.
I set all of the gpio to input via P0,R8 = 0, and then read back from address 119. …
Part Number: TAS5756M Other Parts Discussed in Thread: TPA3118D2 , TAS5766M
Hello, Use Case: PVDD: 25VDC ± 0.25VDC Output Configuration: PBTL Rload: 2.7ohms Gain/Switching Frequency: 26dBV, 768kHz We have a several units of TAS5756M devices who are tripping…
Part Number: TAS5756M Other Parts Discussed in Thread: TPA3118D2 During stressful playback (high levels but still within device capability, tone), we are experiencing faults from the TAS5756M. I understand there is (frustratingly) no way to tell the source…
Part Number: TAS5756M Hi TI,
Is there a plan to upstream linux driver for TAS5756M? I see the attempt was made some time back [0], but currently it is not available in upstream linux.
Thanks, Sameer.
Part Number: TAS5756M Other Parts Discussed in Thread: , TAS5805M , TAS5766M
Hi. We're designing custom PCB that TAS5756M is used. TAS5756M will be controlled via I2C by MCU that mounted on this PCB.
We wanna tune the Hybrid Flow of it. We know that…
Part Number: TAS5756M Other Parts Discussed in Thread: TAS5754M Dear TI-team,
We want to use the TAS5756M in I2S master mode. Therefore, we provide either 24.576MHz or 22.5792MHz as master clock depending on sample rate family to pin 22, MCLK. Once we…
Part Number: TAS5756M Tool/software: Code Composer Studio Hi:
TAS5756 is slave mode as 3-wire PCM mode. I2S data format is 2chans、 16bits、LRclk48KHz、bclk 1.536MHz、mclk 24.576MHz.
We have bidirectional i2s data communication, and we also have four…
Part Number: TAS5756M These are the headings from the main product pages. But looking at the datasheets, the power handling in both mono and stereo seems to be identical. I am aware that (supposedly) the only difference is the modulation scheme, but is…
Part Number: TAS5756M Hi,
We are developing a new project using TAS5756M, we only have a custom board. How to dump .cfg files from PPC2 without PurePath MotherBoard and TAS5756MEVK?
Thanks.