Part Number: TAS5756M Sorry if I overlooked something that should be obvious:
What register determines which I2S channel is sent to playback on PBTL configuration? I expected it to be R42, but changing that value has no effect. (We're using quad speed…
Part Number: TAS5756M Can you please tell me which of the ground pins are most associated with the DAC chip output buffer ground in the front end-die of the TAS5754/6M? This should be available in the bonding diagram of the device. If you could provi…
Part Number: TAS5756M Other Parts Discussed in Thread: TPS54341 Hello,
I'm facing an extrange problem using a dual TAS5756 Configuration.
Both are in dual stereo configuration no make it easier, both connected to same I2S signals, same clock, etc…
Part Number: TAS5756M Other Parts Discussed in Thread: TAS2557 , , PCM5242 Hello,
Some time ago we bought the Evaluation kits for TAS5756M, TAS2557 and PCM5242.
We applied for the software for all of those. Until now we only got access for the PurePath…
Part Number: TAS5756M Other Parts Discussed in Thread: TAS5754M Hi.We're designing the custom PCB that TAS5756M is used(PBTL mono structure). On our PCB, external ADC is exist to convert analog input to I2S. We refferd the datasheet of TAS5754M and…
Part Number: TAS5756M Other Parts Discussed in Thread: TAS5754M Hi team,
There is a problem with the customer's TAS5756MEVM. Now, customer uses the register configuration of TAS5754M (mainly the content of page 0) to configure the TAS5756M. Is this ok…
Part Number: TAS5756M
Team,
Customer is observing a strange issue on the custom PCBs:
TAS5756M is used as I2S master and interfaced to an MCU (that decodes MP3 and output to I2S).
-At 44.1 ksps the system always work (whether or not it is mounted in…
Part Number: TAS5756M Tool/software: Code Composer Studio Hi,
I'm used the TAS5756 and used BT audio module to I2S master/ TAS5756 to I2S slave.
So I follow these sequences that hope can solve the issue of send 8KHz LRCLK and the TAS5756 cannot speak…
Part Number: TAS5756M Tool/software: Code Composer Studio hi:
one project of our company will use TAS5756 to construct a stereo speaker.currently we stuck in the step of configuring TAS5756. We are recommended to configure 5756 with PPC2.
We have a…