Part Number: TPS43061 Other Parts Discussed in Thread: TINA-TI , , TAS5760MD Tool/software: TINA-TI or Spice Models Hello there! Is it possible to use the TINA-TI simulator to simulate voltage/current supply transients caused by an Audio signal when using…
Hi Kim,
Please check TAS5760MD, which supports hardware control mode and headphone channel. But BQ or DRC programming is actually not supported. If you are interested in this device and have more question on it, please post another question in E2E forum…
Other Parts Discussed in Thread: TAS5760MD Hi Expert,
When I run my system, in some music, the PVDD can find 20A current around 3mS. The PVDD source is from battery. Does it impact TAS5760MD reliability? Thanks!
Hi, Alex,
Your comments are correct, PPC1 is used for the TAS5760MD and PPC2 for the TAS5756M. Right now there is no PPC3 app for any of these devices.
Best Regards,
-Diego Meléndez López Audio Applications Engineer
Hello Andy -san,
This means the output voltage just before clipping or the output voltage that starts clipping.
It is the data before you get advice on measurement conditions from you.
Please to see below.
TAS5760MD DATA
TPA3118D2 DATA
It is the data…
Other Parts Discussed in Thread: TAS5760LD , TAS5760MD , TAS5760L Hi folks,
In TAS5760LD datasheet, there are two THD+N vs Output Power graph in the same condition.
For example Figure 5 and Figure 6 in page 14, as below picture:
What's the difference…
Other Parts Discussed in Thread: TAS5760MD , TAS5706B , TAS5756M , TAS5760M , PCM1792A , TPA3132D2 , PCM5122 , TAS5754M Hello,
We are currently designing an audio streamer that must meet the following requirements: -stereo 2x 20W output on 8 or 4 ohms speake…
OK, I've figured out my problem. The TCA6424A I/O expander must be reconfigured for using with the TAS5760xxEVM.
So I added the following code in the Device_eventHandler.c file.
// PPCMB I2C Expander
// Port 2
i2c8_write(TCA6424A_ADDR…
Hi, Arun,
If analog input is required, our only option is TPA3004D2.
If you can use I2S input, we have many parts that can fit - for example, TAS5760MD.
-d2
Other Parts Discussed in Thread: TAS5760M , TAS5760MD , PCM5100A Hello,
I am trying to use the TAS5760M (or TAS5760MD) in an audio amplifier that takes digital input. The device needs a stereo headphone output and a stereo speaker output. To reduce cost…