Part Number: TAS5805M Other Parts Discussed in Thread: TAS5805 Tool/software: Hi, Team
Customer is checking with us about the min_height value of the TAS5805.As you can see from the datasheet as below, TAS5805M didn’t have such value. TAS5805M only have…
Part Number: TAS5805M Other Parts Discussed in Thread: TAS5805 , , TAS5828M Tool/software: Mr. Yang,
I am using TAS5805 in my system. I am trying to confirm the logic. At the power up, if I just want to verify my TAS5805 is online and setting DEVICE_CTRL_1…
Part Number: TAS5805M Other Parts Discussed in Thread: PUREPATHCONSOLE Tool/software: My request for access to PUREPATHCONSOLE has been denied, I would like to know what information was judged to be wrong that led to the rejection
I have checked that the…
Part Number: TAS5805M Tool/software: Hi,
In our project, we're using the TAS5805M in BTL mode with a maximum output of 1W per channel.
However, when PVDD is set to 24V, the temperature rises above 150°C until the amp triggers thermal protection.…
Part Number: TAS5805M Tool/software: Hi,
We use the TAS5805M for our audio Amplifier design, now, we test the drive but there are no audio output, we read the register 0x3h=00 that TAS5805M is on the sleep mode.
We have below support need:
1. Can you provide…
Part Number: TAS5805M Other Parts Discussed in Thread: TAS5805 Tool/software: PPC3 software was used to generate a.h file containing EQ and crossover, write TAS5805 and check the verification code,
and measure the voltage frequency response curve at the…
Part Number: TAS5805M Hi ti team,
Using TAS5805M for mono 1.1. Split the low frequency range to 60HZ-4KHZ, and discard the rest of the frequency range. We found that the TAS5805M frequency drops suddenly at 2KHZ-3KHZ. What is the reason for this? Under…
Part Number: TAS5805M Tool/software: Hi team,
Customer has mute issue occasionally since it might be caused by automute state.
They set below commands by entering and exiting from mute. They set automute register like : 0x50 = 0x07(Independent L,R, Enable…