Part Number: TAS5806M Hello.
I have a question about the EEPROM.
If you look at the TAS5806MEVM, the EEPROM is connected as shown in the picture below.
1. Can I put DATA such as DRC and EQ TUNING in the EEPROM and drag it and use it?
2. On the PUREPATH…
Part Number: PUREPATHCONSOLE Other Parts Discussed in Thread: PUREPATH-CMBEVM , TAS5806MEVM Currently, I am trying to output sound from speakers using PUREPATH-CMBEVM, TAS5806MEVM. I want to read and play a wav file using purepath console3's Audio Player…
Part Number: TAS5806M Hi TI experts,
We are using the TAS5806MEVM to test the DRC control.
Set DRC as below.
We are measuring the frequency response. however, this is different from the PPC3 graph. There was a gain at 250Hz and 15kHz.
See the Cyan color…
Part Number: TAS5806MD Other Parts Discussed in Thread: TAS5806MEVM Hi,
I designed my circuit according to TAS5806MEVM User's Guide page 7. The LC filter is realized with 4.7uH (Mfr.Pn: TYA40204R7M-10) and 0.68uF. PWM switching frequency is 384kHz and…
Part Number: TAS5806M Hi TI experts,
Regardless of the input level, We want to set the 80 Hz band to the same output.
The attached file has the graph we want and the TAS5806M output graph. Please check the attached file.
Request.xlsx
We tried to attach…