Part Number: TAS5825P
Hi:)
-
According to the "TAS5825P Hybrid-Pro User Guidance", when there are several TAS5825P ICs with the Hybrid-Pro feature enabled the Hybrid-Pro outputs should be set to 'Open-Drain' and connected together, along with…
Part Number: TAS5825P Hi,
We have finished TAS5825P tuning.
May I know any way to dump TAS5825P setting to any format, that we can easy let MCU set to TAS5825P when system boot up?
Thanks!
Jeff
Part Number: TAS5825P Hi team,
For the TAS58xx AMP IC, what is the minimum speed of I2C that it can support? the D/S says maximum 100kHz for the slow mode.
My customer wants to use 70kHz speed for the I2C. Can you help if this could work?
Thank you…
Part Number: TAS5825P Other Parts Discussed in Thread: TAS5825M ,
Hi:)
I am currently working on a design that uses 2x TAS5825P + 2x TAS5825M and have now come to the point where selection of a suitable Boost-Converter is required.
However I did not…
Hi Jesse, Please refer my comments.
Jesse Ji said: you test directly from sdout? am i understanding correct?
No, Just tested at the actual output.
Jesse Ji said: also, the THD been improved, you mean it will become same between 44.1k and 48k if setting…
Part Number: TAS5825P Other Parts Discussed in Thread: TAS5822M , TAS5825M Hi Team,
My customer is designing TAS5825P and built a prototype. However they are facing a problem when connecting EVM with their proto-board to use GUI's End System Integration…
Part Number: TAS5825M Other Parts Discussed in Thread: TAS5825P Hi team,
What is the main differences between TAS5825M and TAS5825P?
Best regards,
Shunsuke Yamamoto
Part Number: TAS5825P hi expert
there is an issue about TAS5825P need your help. At this application, set sample rate as 44.1k(0x28 = 0x08), while the device state from standby to wakeup, there is no output of TAS5825p.And the register shows clock default…