Hello Luis,
My request for PPC3 is still in limbo! Do let me know it its possible to use TAS5828M without PPC3 in stereo mode? Or PPC3 is must have to use TAS5828.
Thanks -Mayuresh
Part Number: TAS5828M Other Parts Discussed in Thread: TAS5805 Hi, Team,
Customer want to know If we use TAS5828+TAS5805 in parallel. Are there any differences between these connection methods?
1. The same SDIN is given to 5805 and 5828
2. SDIN is given…
Part Number: TAS5828M Hi team,
The datasheet shows that PVDD under voltage error threshold is at 4V.
Will this be triggered everytime PVDD is ramping (start-up) and shutdown?
Thanks,
Luke
Part Number: TAS5828M I am using thermal paste between top of the IC and the external top mounted heat sink. My reading suggests that the heat sink needs to make actual contact with the IC. Is this correct? I am concerned about the weight of the heat…
Part Number: TAS5828M Other Parts Discussed in Thread: TAS5825M , Hi team,
In TAS5825M ProcessFlow(slaa786a), it says "Input signals are converted to 88.2kHz or 96kHz" regarding SRC. Is this SRC's function in TAS5825M same with the one in TAS5828M?…
Part Number: TAS5828M Hi team,
What is the difference in operation when the SRC control panel in PPC3 is set to [As Input][44.1kHz][48kHz]?
Best regards,
Shunsuke Yamamoto
Part Number: TAS5828M Hi team,
Is it possible to bypass Input Mixer when using stereo mode? When we look at the advanced mode, it looks like it is adding something together even in stereo mode. Is it impossible to bypass Input Mixer completely?
Best…
Part Number: TAS5828M Hi team,
In Datasheet, sampling frequency can be supported up to 192kHz. but 192kHz sampling frequency is not available in PPC3. How do we choose it?
Best regards,
Shunsuke Yamamoto
Part Number: TAS5828M Hi,
I am trying to run TAS5828M in hardware mode. There is no output. Below are some details I can share.
1. Connected R6 (Pin 13 - ADR (HW_MODE) to DVDD with 0Ohms resister to switch to Hardware mode. Voltage on ADR pin is 3.3V…
Part Number: TAS5828M Hi There,
SDOUT is a feature of the TAS5828M that we will use for subwoofer output. 1.Can this be configured to be SPDIF format? 2.In the case we use AutoDetect for input sample rate, then how can we use the SDOUT feature? Let…