Part Number: TAS6422E-Q1 Other Parts Discussed in Thread: TAS6422-Q1 Tool/software: Hi Team,
We are using the TAS6422QDKQRQ1 in our design for the product.
Following are the Amplifier configuration done through I2C 1. Mode Control Register 0x00 = 0x00…
Part Number: TAS6422-Q1 Tool/software: Hi support Team,
When we measure the FFT graph of the ECU, the frequency spectrum after 3000 Hz is not as expected. We are trying to identify the correct FFT graph by comparing the ECU used with another amplifier…
Other Parts Discussed in Thread: TAS6422-Q1
Hi, Support Team
Q1: if TAS6422-Q1 output disconnect to speaker, the TAS6422-Q1 have alert is trigger from FAULT pin?
Q2: under voltage/over voltage trigger is from FAULT pin?
note: our client verify DC diagnostic…
Part Number: TAS6422-Q1 Hi TI Support Team,
The configuration of the amplifier remains default setting for all register so it begins PLAY mode for two channel.are active and used load is 4 ohm speaker. I read only 0x0C register for the aim. Let's con…
Part Number: TAS6422E-Q1 Hi Team,
Customer is using TAS6422E-Q1 in mass production and they found few IC has lower Vout voltage in OUT_2M and OUT_2P.
Most IC are 16.1~16.5V and only a few are 15.2~15.5V, they removed the speaker and result are the same. …
Part Number: TAS6422E-Q1 Dear TI experts,
My customer considers TAS6422E-Q1 for their new project.
They want to know to limit output power of TAS6422E-Q1.
It can make output power up to 75W, but they want to limit output power to 5W, and steady 5W even…
Part Number: TAS6422-Q1 We are bench testing our custom TAS6422-Q1 board. We are doing power / heat tests by playing 1KHz sine waves via TDM, with the amp outputs connected to 100w 4R resistors.
At lower amp gains everything is good, we get an excellent…
Part Number: TAS6422-Q1 Other Parts Discussed in Thread: LM5123-Q1 , TIDA-020033 , TAS6584-Q1 , CC3235SF We have a product using this amplifier and it is up and working well. However we intended it to woks in 2 battery applications
as one finds in semi-trucks…
Part Number: TAS6422E-Q1 Hi, TI Support Team
I want to know how long it takes for the out_1P/1M/2P/2M to become 50% PVDD after /STANDBY becomes Hi at VDD/VBAT/PVDD power supplied condition.
If the timing of when out_1P/1M/2P/2M becomes 50% PVDD varies…
Part Number: TAS6422E-Q1 Hi team,
We configured TAS6422 as PBTL mode, we would like to play the ch2 of I2S input. But register 0x3 only offer TDM slots selection,
So my question is how to select I2S ch2 at PBTL mode?
Thanks
BRs
Kian