Other Parts Discussed in Thread: TAS6422-Q1
Hi, Support Team
Q1: if TAS6422-Q1 output disconnect to speaker, the TAS6422-Q1 have alert is trigger from FAULT pin?
Q2: under voltage/over voltage trigger is from FAULT pin?
note: our client verify DC diagnostic…
Part Number: TAS6422E-Q1 Hi Team,
Customer is using TAS6422E-Q1 in mass production and they found few IC has lower Vout voltage in OUT_2M and OUT_2P.
Most IC are 16.1~16.5V and only a few are 15.2~15.5V, they removed the speaker and result are the same. …
Part Number: TAS6422E-Q1 Dear TI experts,
My customer considers TAS6422E-Q1 for their new project.
They want to know to limit output power of TAS6422E-Q1.
It can make output power up to 75W, but they want to limit output power to 5W, and steady 5W even…
Hi
Göknur Setrekli said: it already can not be find the channel state in any time, too. Am I wrong?. Can you explain in detail above that you said?
If the device already into PLAY state, and open load appears, then indeed there's no way for the device…
Part Number: TAS6422E-Q1 Hi, TI Support Team
I want to know how long it takes for the out_1P/1M/2P/2M to become 50% PVDD after /STANDBY becomes Hi at VDD/VBAT/PVDD power supplied condition.
If the timing of when out_1P/1M/2P/2M becomes 50% PVDD varies…
Part Number: TAS6422-Q1 We are bench testing our custom TAS6422-Q1 board. We are doing power / heat tests by playing 1KHz sine waves via TDM, with the amp outputs connected to 100w 4R resistors.
At lower amp gains everything is good, we get an excellent…
Part Number: TAS6422-Q1 Other Parts Discussed in Thread: LM5123-Q1 , TIDA-020033 , TAS6584-Q1 , CC3235SF We have a product using this amplifier and it is up and working well. However we intended it to woks in 2 battery applications
as one finds in semi-trucks…
Part Number: TAS6422E-Q1 Hi team,
We configured TAS6422 as PBTL mode, we would like to play the ch2 of I2S input. But register 0x3 only offer TDM slots selection,
So my question is how to select I2S ch2 at PBTL mode?
Thanks
BRs
Kian
Part Number: TAS6422E-Q1 Other Parts Discussed in Thread: TAS6424E , TAS6424E-Q1 ,
Hi, Support Team
Please help to review schematic as below chart:
1. about PIN22 and PIN23 schematic:
if sametime we use TAS6422E and TAS6424E set up the same address, have…
Part Number: TAS6422E-Q1 Dear TI experts,
My customer now tests their own PCB with TAS6422E-Q1.
First they applied 3.3uH for the inductors below. (L38, L39, L40, L41)
They found that there is a sine wave with some noise, and they changed the value of…