Part Number: TAS6422E-Q1 Dear Support Team
I would like to get the support to review the schematic for TAS6422EQDKQR. Please let me know your feedback on this
VIN: 14V
Output : 20W power for Each Channel
TAS6422EQDKQR _Sch_Review.pdf
Regards,
Bala
Part Number: TAS6422E-Q1 Dear Team, i'm looking for driver for ' TAS6422E ', on linux kernel-5.4 for the SOC-qam8295p.
I'm unable to find in OpenSource kernel. Pls let me location of the driver source.
Regards
K.Mani
Part Number: TAS6422E-Q1 Other Parts Discussed in Thread: TAS6424-Q1 Hi team,
Is there Temperature foldback feature in TAS6422E-Q1?
Temperature foldback means the device automatically limit the volume when junction temperature exceed the predefined threshold…
Part Number: TAS6422-Q1 Hello TI Team,
This is an continuation of the same case from last year. We finally got around to improve the cooling, replace the output inductors and more, but the tas6422 still goes into overcurrent on channel 2 if we have both…
Part Number: TAS6422E-Q1 Hi team,
I'm a bit confused by the dialogue in the question related to this thread. It seems that the heat sink can be electrically isolated from the heatsink (no current flow) but must still have a nearby connection to ground…
Part Number: TAS6422E-Q1 Other Parts Discussed in Thread: TAS6422-Q1 Hi Team,
The customer applied TAS6422E-Q1 to VESS.
Spec : 150 W, 10% THD Into 2 Ω at 25V PBTL
Customer checked the operation until input, but TAS6422-Q1 doesn't output.
MCLK…
Part Number: PCM6020-Q1 Other Parts Discussed in Thread: TAS6422-Q1 Hi, Support Team
our software team have a question:
if ADC(PCM6020-Q1) can read voltage vaule.
how to mapping digital signal related voltage value?
function block:
if any suggestion…
Part Number: TAS6424E-Q1 Other Parts Discussed in Thread: TAS6424E
Hi MPA BUs,
This is Koki Tsushima. Thank you for your continuous support.
I want to ask you that does TAS6424E, TAS6424M or TAS6422 remember register setting after goes into standby…
Part Number: TAS6422-Q1 Other Parts Discussed in Thread: TAS6424 Hi,
I understand that TAS6422 is digital input 2-channel Class-D amp, not 4-channel Class-D amp. Therefore, it has many reserved bits in the registers for TAS6422. Then, I have a qestion. …
Part Number: TAS6422E-Q1 Hi,
I am developing A2B product using TAS6422E-Q1.
When I set the setting to 48 K H z, there is no sound, and the sound is output at 44.1KHz.
Please see the settings below and let me know what settings I am making mistakes.
The…