Part Number: TAS67524-Q1 I have some questions regarding the audio interface configuration of TAS67 6 24. (It is not TAS67524.)
FS frequency / number of TDM slots Is there a register that explicitly sets the FS frequency and the number of TDM slots…
Hi Shota,
Thank you for the well-organized question!
Shota Ueyama said: the length of the DC diagnostic waveform is long.
Could you please define "long"? The typical DC diag time is 155ms, I have measured the DC diag time (SL/OL part), and they…
Part Number: TAS6754-Q1
The datasheet says: Input sample rates: 44.1, 48, 96, 192kHz
Is it possible to use 8 KHz sampling rate on the TAS6754-Q1 ot TAS67524?
If not, what multi-channel audio amplifier can you recommend that can do:
TDM-8 or…
Hi,
Thank you for your feedback.
I am planning to consider the TAS67524-Q1 for our new design and would appreciate clarification on the following points:
1. Is there any software compatibility difference between the TAS67524-Q1 and the TAS5760M…
Hi,
thanks for the information. How do I configure the TAS67524-Q1 for CBC level of 8A? The datasheet of the TAS67524-Q1 states 6.5A(min) ... 7.0A (typ) for OC Level 4.
What is your suggetion on how to continue the 2Ohm Test with >45W with the TAS6754…
Part Number: TAS6754-Q1 Other Parts Discussed in Thread: TAS67524-Q1 Tool/software: How to get to know which silicon version of chips are installed from which registers?
version 1p1 of TAS6754-Q1
version 2p0 of TAS6754-Q1
the chip of TAS67524-Q1…
Dear Leo,
Sorry for late reply.
It is the project of AVN (Audio/Video/Navigation) of the car.
I understand tat TAS67524-Q1 is newer and recommended device. Then the schematic is still valid for TAS67524-Q1 and have no problem?
Best regards,
…
Part Number: TAS6754-Q1 Other Parts Discussed in Thread: TAS67524-Q1 Hi. I want to start designing the TAS6754-Q1 amplifier into a new product. I have searched for the Linux drivers but I cannot find them. How do I obtain them ?
Part Number: TAS6754-Q1 Other Parts Discussed in Thread: TAS67524-Q1 Tool/software: #1 We are checking whether all abnormalities that TAS67524-Q1 level down or shut down can be notified by the Fault pin. When leveling down or shutting down, what kind…
Part Number: TAS6754-Q1 Other Parts Discussed in Thread: TAS67524-Q1 , Tool/software: Hello experts,
My customer sees audio output stopping with 2ohm speaker and big volume. They use TAS6754-Q1 EVM and they will use TAS67524-Q1 in MP.
Temperature…