Part Number: TCAN4420 Other Parts Discussed in Thread: TCAN1042DEVM , Team,
can TCAN1042DEVM be used for TCAN4420?
http://www.ti.com/tool/tcan1042devm
Thanks,
A.
Part Number: MSPM0G3507 Other Parts Discussed in Thread: TCAN1042DEVM Dear TI,
I am debugging following example code " mcan_message_rx_LP_MSPM0G3507_nortos_ticlang " to receive the data from my python script.
( python script is interface with ST…
Part Number: MSPM0G3507-Q1 Other Parts Discussed in Thread: MSPM0G3507 , TCAN1042DEVM
Hello TI Team,
I am facing a problem regarding CAN transmit signal detect on CRO.
I am using " mcan_multi_message_tx" example code from "mspm0_sdk_1_20_01_06" in MSPM0G3507…
Part Number: AM625 Other Parts Discussed in Thread: SYSCONFIG , SK-AM62 , TCAN1042DEVM Does the processor SDK Linux support MCAN module (CAN and CAN FD)?
There is no mention of MCAN module in the latest processor SDK Linux (08.03.00.19) documentation.
…
Part Number: TCAN1042H Other Parts Discussed in Thread: TCAN1042DEVM , TIDA-01487 TCAN1042DEVM schematic is described termination resistor size:0603 on 120Ω.
Is this size also recommended for 60Ω condition?
TIDA-01487 is using 125mW resistor…
Dear Max
1. Sorry, I had said wrong, it's not IEC 61000-4-2, it is SAE J2962-2.
Could the device EVM pass the SAE J2962-2 ESD ? I want to test the EVM as below:
http://www.ti.com/tool/ TCAN1042DEVM
2.As you said, the device EVM could pass the IEC 61000…
Other Parts Discussed in Thread: TCAN1042DEVM , TIDA-01429 , TCAN1042-Q1 Dear gents,
looking for CAN interface development/eval. board for automotive radars samples that can send and read out values from commercial samples of radars like the one in attachment…
Michael,
A simple set-up would be to get a CAN transceiver evaluation board, power it up, connect the CANH/CANL lines to your system, and then drive the wake-up pattern on the TXD input to the transceiver using a function generator. Here's an example…
Part Number: TCAN1051HGV Hello,
My customer would like to use TCAN10xx Controller Area Network (CAN) Evaluation Module: http://www.ti.com/tool/tcan1042devm#buy to test TCAN1051HGVDR.
Is it something feasible? Because in the product folder I see this…