Part Number: TDC1011 Other Parts Discussed in Thread: TIDA-00322 , TDC1000 , TDC1000-C2000EVM , TUSS4470 , TDC7200 I am creating a novel ultrasonic device, I will be using the TDC1011 analog front end AFE which is capable of producing 4mhz. This AFE produces…
Part Number: TDC1011-Q1 Hi Expert,
TDC1011-Q1 is used in customer's system. For Unused RTD2, Could you give us a recommendation for this? Thanks.
Best Regards
Songzhen Guo
Part Number: TDC1011 Hi
In the production line test, we are now looking a way to simulate the sensor disconnect condition to test if our TDC1011 design works fine or not.
Thus we will need to put a switch IC in between TDC1011 and sensor to disconnect…
Part Number: TDC1011 HI,
I want to drive 8 TDC-1011 by hardwiring the SPI interface pins to a single micro controller for configurating programming. Will there be any problem or do I need to use a buffer in between to enhance drive capability? Please…
Part Number: TDC1000 Other Parts Discussed in Thread: TDC1011 Hi Ti team,
Could you pls help us check below question?thanks!
We plan to use tdc1000 and tdc1011
Ultrasonic transmission and reception, used to test the thickness of fat, please help to…
Part Number: TDC1011 Other Parts Discussed in Thread: TDC1000 , What are the differences between these devices? I am am looking through the datasheets and they appear to be very similar.
Hi Bharat!
For the current version of our product we've decided to accept the additional sleep current draw of the device to simplify the design. If we put the switched power rail back into the design, we'll switch both VDD and VIO on the TDC1011.…
Part Number: TDC1011 We have a question. The water level test example on TI's DEMO board and application documentation is to place the ultrasonic probe under the water tank to check the liquid level. However, the customer's application should …
Part Number: TDC1011 Hi Bharat,
Thank you for your reply. I configured the RX path, but I still can not see any amplification. Any clue?
Thank you in advance.
BR.
Aitor.
Part Number: TDC1011 Hello,
I am woriking with TDC1011 in a project where 1MHz ultrasonic transducers will be used to measure some media concentration.
However, at this point of the project I replase the ultrasonic signal by a 1MHz sine wave from a GFG…