Part Number: TDC1011 Other Parts Discussed in Thread: UCC27531 , , PGA460 , TDC7200 , TLV61046A
Hi,
i am using the TDC1011 with the UCC27531 to drive my transducer.( TDC1000-GASEVM )
I have a step up converter that generates 28V.
Everything works fine but…
Part Number: TDC1011 I want to use SPI interface of 8 TDC-1011 with a microcontroller for communication. Will there be any problem? What are the SPI electrical specifications of TDC-1011? Please help me.
Regards,
Sundar
Part Number: TDC1011 Other Parts Discussed in Thread: DRV2700 , Hi,
i want to use the TDC1011 IC with DRV2700 to drive a transducer with 40kHz.
I can use an opamp to take the TX(TDC1011) and make it differential to the inputs of DRV2700.
The DRV2700 will…
Part Number: TDC1011 I need to drive a transducer with 1200V for its optimum performance. Would I be able to configure the TDC1011 TX signal as in the circuit below to drive a centre tap transformer and feedback the TDC1011 RX signal?
Part Number: TDC1011 Other Parts Discussed in Thread: TDC1000 , I have a simple proximity sensing application where I just need to detect the distance to an object through air.
It seems like the PGA450 is essentially a TDC1011 with an 8051 core onboard…
Hi Pambo,
For your max range of 20cm, both the PGA460 or TDC1011 are feasible candidates, even with a lower driving voltage. If you find that the TDC1011 can provide more efficient power savings, I see no reason not to consider this device. I have a…
Part Number: TDC1011-Q1 Other Parts Discussed in Thread: TDC1011 , TDC1000 I have a system built with TDC1011 initially designed for 1MHz ultrasound transducers. I'm wondering if it will be possible to continue using this board (with TDC1011) for 5MHz transducers…
Part Number: TDC1011 Other Parts Discussed in Thread: TDC7200 , Dear Vishy Viswanathan,
I'm developing automatic water-supply reservoir for a cow using TDC1011 , TDC7200 and steminc's SMFM21F1000.
Currently, I need some advice to change an mounting…
Part Number: TDC1011 My input signal is connected to both the COMPIN pin of the TDC1011 and a ADC. Don't want the TDC1011 to affect the input signal. Can't fin the input impedance of the COMPIN. Can probably isolate it with a resistor also.
Part Number: TDC1011 Other Parts Discussed in Thread: TDC1000 Hi,
My application is measuring the level of water in a water tank with the ultrasonic transducer mounted on the top cover of the water tank (on the inside).
Detection range is from 10 cm to…