Part Number: THS3201 Other Parts Discussed in Thread: THS3491 , , LMH6703 Dear TI team, I intended to use TH3201 in my design, but just recently I noticed that you do not recommend using it for new designs and it is recommended to use THS3491 instead…
Part Number: LMH6703 Other Parts Discussed in Thread: THS3491
Tool/software:
Dear Technical Support Team,
I'd like to confirm to use ADI's method with LTSpice, but it seems not to work for open loop gain(FB/INM).
The gain results in a gain of…
Part Number: THS3201 Other Parts Discussed in Thread: THS3491 Tool/software: Dear TI team,
I am currently testing the THS3201 using the inverting amplifier configuration suggested in the datasheet, ... but I am encountering unexpected behavior. When…
Part Number: LMH6611 Other Parts Discussed in Thread: THS3491 , OPA2675 , OPA891 Tool/software: Hi team,
Do we have higher current amplifier but with similar spec with LMH6611 ? LMH6611's 100mA drive current is not enough.
Part Number: SN74AUP2G17 Other Parts Discussed in Thread: THS3491 , TLV1871 Tool/software: Hi,
We are developing a ground based receiver with different inputs and the outputs. Can you suggest the protection circuit/IC which is support for the over voltage…
Part Number: THS3001 Other Parts Discussed in Thread: THS3491 Hi I see from the datasheet that the DGN package has only 4.7 Degrees C/W thermal resistance to case. Is this the resistance to the thermal slug ? Also does anyone have the thermal resistance…
Part Number: THS3001 Other Parts Discussed in Thread: THS3491 Looking for data at Vcc = + 15 V, V_o(pp) = 20V or greater, with Gain = 3, 5, and 10. Or the closest data available.
Part Number: OPA2890 Other Parts Discussed in Thread: OPA890 , THS3491 , LMH6703 Tool/software: Dear Technical Support Team,
What is the maximum frequency of the OPA890 for square wave?
10MHz seems to operate correctly, however 250MHz (500Mhz) is…
Part Number: THS3091 Other Parts Discussed in Thread: THS3061 , , THS3491 I'm considering using the THS3091 or THS3061.
How do these two parts compare in regards to intermodulation distortion?
Is there a model/simulator that would allow simulation…