Part Number: SK-TDA4VM 1. Download ti-processor-sdk-linux-adas-j721e-evm-09_02_00_05-Linux-x86-Install.bin and install.
2. execute sudo ti-processor-sdk-linux-adas-j721e-evm-09_02_00_05/bin/create-sdcard.sh, create SD rd with prebuilt Image in the sd…
HI Minh
I am not sure whether it will work or not, you can try changing the drive strength value in the dtsi also try using different speed mode by modifying the dtsi.
Regards Diwakar
Other Parts Discussed in Thread: TDA4VM Hi Ti
I'm working on bring up an ISX016 Cam with ub913 and Ub964 deserialiser with ti-processor-sdk-rtos-j721e-evm-07_01_00_11.
Please find the application logs for your reference.
/cfs-file/__key/communityserver…
Hi,
Sorry for the delay in response here.
You had mentioned earlier that the eDP output from the EVM is fine whereas the issue is from the HDMI input from the infotainment board.
From the displays attached, there is no issue with the DSS IP as you see…
hello,
The data is not coming up on the CAN as before.
https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1216687/faq-j7200xsomxevm-how-do-i-enable-can-with-linux-driver-on-j7200 .
I am trying to build PSDK 8.5 in order to apply…
Hello,
ST T said: yeah! just out of curiosity.
do you mean this: https://www.ti.com/lit/ug/spruj62/spruj62.pdf?ts=1710380362594&ref_url=https%253A%252F%252Fwww.ti.com%252Ftool%252FJ784S4XEVM
(from https://www.ti.com/tool/J784S4XEVM )
Sure .. I can…
Part Number: TDA4VM Dear TI Support,
The following error occurred during make qnx_fs_create.
/home/nahyoun/ti/ti-processor-sdk-rtos-j721e-evm-07_01_00_11/psdkqa/qnx/bsp/images/ifs-j721e-evm-ti-spl.raw
It says there is no ifs-j721e-evm-ti-spl.raw file…
Part Number: AM3352 Hi,
I installed ti-processor-sdk-linux-am335x-evm-09.01.00.001-Linux-x86-Install.bin at my ubuntu 22.04 (LTS) 64bit virtual machine (VBOX)
see below
howdoudo@howdoudo-VirtualBox:plugin$ uname -a Linux howdoudo-VirtualBox 6.5.0-17-generic…