Hello Sahaj,
The beam spread is mainly associated with the transducer. Different manufacturers offer different FOV angles. There are a couple of other ways that you can increase the range for your application:
1. Higher frequency signals attenuate faster…
Dear All,
I'm reading in TIDA-00322 Test Results , Paragraph IV / Point B.2. : Connect the transducer TX/RX wire to J3.P8, and the sensor's ground to J3.P10.
According to Schematic/Block Diagram , connecting the transducer between P8 and P10 leads…
Other Parts Discussed in Thread: TDC1000 , TIDA-00322 I am evaluating the performance of TDC1000. Can you give the source code of TIDA-00322 on C2000 processor?
Part Number: TDC1000 Other Parts Discussed in Thread: TUSB3410
Hello experts,
I have started working on ultrasonic vehicle fuel level sensor. For this project i have selected the TDC1000 as AFE and C2000 as the MCU. As I understood, I have to connect…
Hello Jeff,
Thank you for your question. Will you be trying to make a liquid level measurement from the outer top of the tank or the inner top part of the tank?
I do have some concerns over operation using a 3.6V battery if the measurement would be taken…
Hi, I have checked the firmware example you suggested, and in the source code there is also the managing of the component LMP91400 that is not present in the schematic of TIDA-00322, so I think it is related to another board. I will wait for your answer…
Hi Minrak,
Both GUI installers contain source code for their respective microcontroller on the EVM. The source code files are available at the install path of the GUI.
C2000 MCU source code is available in TDC1000-C2000EVM GUI v1.2.0.83 (TIDA-00322)…
Great, you answered almost everything I needed to know. Thank you,appreciated it..
1. It looks like the TIDA-00322 is not for sale. Do you have a full system like this that can be purchased?
2. If I decided to use the TDC1011, what alternative I can…
Hi Mark,
All of the firmware source code and drivers are included in the TDC1000-C2000EVM GUI v1.2.0.83 (TIDA-00322) (Rev. B) download.
If what you are seeking is not included in this download, you may need to contact the TUSB3410 team for further details…
Hi Songzhen,
The customer can use the TDC1000-C2000EVM GUI to download the register configuration of the TDC1000. Here are the steps:
In the GUI, click the "TDC1000" tab at the top.
In the bottom right corner of the page, click the button …