Hi Akeem,
The option to order the TIDA-00322 board is not avaiable.
If i could find this board is sure that is compatible with the TX output signal of the TDC1000-C2000EVM?
The TUSS4470 and TUSS4440 have any EVM easily compatible with the TDC1000-C2000EVM…
Yumiko-san,
The TDC1000's bit field named "NUM_RX" can be set to monitor for a fixed 1 to 5 STOP pulses, or an indefinite number of STOP pulses to capture >5 STOP events. So yes, it is possible to capture 7 or more STOP pulse events. …
Hi Dennis,
If you are using a 1MHz transducer, you may want to consider using the TUSS4470 instead of the TDC1000 for a time of flight distance measurement. More details here: https://e2e.ti.com/support/sensors/f/1023/t/748143
What are the specific system…
Part Number: TMS320F28035 Other Parts Discussed in Thread: TIDA-00322 , , TDC1000-C2000EVM , TDC1000 Hi, I'm having issues connecting the GUI interface to the TMS320F28035. I'm using the TIDA-00322 reference design, and connecting using an FTDI cable…
Part Number: TDC1000-C2000EVM Other Parts Discussed in Thread: TDC1000 , TUSS4470 , PGA460 , TUSS4440 , TIDA-00322 , UCC27531-Q1 Good morning,
I am a first time user of ultrasound and so likely out of my depth but hopefully you can help with a simple application…
Hello Malay,
Typically we can measure the level sensing using the EVM upto a 1m. For higher level measurement of >1m we will need to level shift the TX pulses to greater voltages. Refer to the TIDA-00322 in the link below:
www.ti.com/.../tidu617a…
Thanks Scott,
We are using the standard Steminc 1 MHz transducer that is packaged with TDC1000-7200EVM.
I was also looking into the schematics of the TDC1000 reference design (TIDA-00322) that proposes a simple boost circuit.
Regards,
Oleg.
For TDC1000 level application, we have tested a range of 2cm to 88cm as part of the following TI design and app note.
www.ti.com/.../TIDA-00322
www.ti.com/.../snaa270
Please check this e2e posting as well
e2e.ti.com/.../467713
Thanks,
Vishy
The BSTEVM circuit of GASEVM is part of the following TI design (for which you can find all the design files)
www.ti.com/.../TIDA-00322
MSP430, TDC1000 and TDC72000 are also part of the following flow meter TI design (again you can find all the design…
Thanks, Vishy. I looked at these reference designs. I am quite new Electronics geek. Do I have to make clone of this whole reference board( TIDA-00322 )? I wanted to make a miniature and cost effective design to fit it into my product. Is there any way…