Part Number: TIDA-010042 Other Parts Discussed in Thread: CSD19531Q5A , LM5109B , MSP-FET Hi Team,
Our customer has a couple of questions regarding TIDA-010042: 1. Why are R45, R45, R55, R56, D8, D9, D10, D11, D12 and D13 not supposed to be populated?
What…
Part Number: TIDA-010042 Hi. I am currently simulating the TIDA-010042 hardware portion in PSpice to validate its use in our use case. For the time being I am giving the pulses to the mosfets directly with VPULSE source (without using gate driver and…
Part Number: TIDA-010042 Hi, The input voltage specification of the design varies from 15V to 60V, which can be used for giving 48V as output. The design implements interleaved buck configuration. How it is able to boost from 15V to 48V with the buck…
Part Number: TIDA-010042 Other Parts Discussed in Thread: BQ24618 Hi, I am designing a portable power station using a reference design given on this link. https://www.ti.com/solution/portable-power-station?variantid=237090&subsystemid=237095
I need…
Part Number: TIDA-010042 Other Parts Discussed in Thread: LM5109 , INA280 , INA240 , LM5009 , LM5168 Hi, I have solar panel with output 15Watt and open circuit voltage 111V. I need to interface with TIDA-010042. TIDA-010042 maximum input voltage is 15 V to…
Part Number: TIDA-010042 Other Parts Discussed in Thread: CC2640R2L , , TIDA-00120 , LAUNCHXL-CC2640R2 , MSP430F5132 , BQ25798 Hi Experts, Good day. The customer is asking.
I am in senior design at Milwaukee School of Engineering and unfortunately, I am unable…
Part Number: TIDA-010042 Other Parts Discussed in Thread: MSP430F5132 , MSP-FET I developed the prototype using the design probided by the TI. Now I want to pragram the (MSP430F5132) present on the TIDA-010042.
How to use MSP-FET to program TIDA-010042? …
Part Number: TIDA-010042 Hi,
-Is it correct that the battery is connected to J5?
-Is it correct that the load is connected to J7?
If so can I:
-connect multiple TIDA-010042 J5 connectors (parallel) to the batterie(s)?
-Can I also connect the load connectors…
Hello,
I am planning to build this reference design but i have a quick question so i can understand if it suits my case.
My battery is 12V lead acid and i have a 12V solar panel.
My first question: I notice that the max charge current for this board…
Part Number: TIDA-010042 Other Parts Discussed in Thread: MSP-FET , , LM5009 , TINA-TI I programmed the required firmware. but the fabricated device is not functioning. kindly suggest a solution.
can any one come provide live solution so that i can finish…