Part Number: TIDA-010042 Hi,
-Is it correct that the battery is connected to J5?
-Is it correct that the load is connected to J7?
If so can I:
-connect multiple TIDA-010042 J5 connectors (parallel) to the batterie(s)?
-Can I also connect the load connectors…
Hello,
I am planning to build this reference design but i have a quick question so i can understand if it suits my case.
My battery is 12V lead acid and i have a 12V solar panel.
My first question: I notice that the max charge current for this board…
Part Number: TIDA-010042 Other Parts Discussed in Thread: MSP-FET , , LM5009 , TINA-TI I programmed the required firmware. but the fabricated device is not functioning. kindly suggest a solution.
can any one come provide live solution so that i can finish…
Part Number: TIDA-010042 I developed the board with all componenets.
but later I saw DNP on few components.
Should i need to desolder those DNP components or shall i leave it as it is.
will there be a problem if i leave it as it is
Part Number: TIDA-010042 Hi,
-Is it correct that the battery is connected to J5?
-Is it correct that the load is connected to J7?
If so can I:
-connect multiple TIDA-010042 J5 connectors (parallel) to the batterie(s)?
-Can I also connect the load connectors…
Part Number: TIDA-010042 Hi,
I studied the TIDA-010042 design which accepts up to 60 V. I want to use a soalr panel which goes up to 70.4 Vmpp so, I guess I need to select a replacement for some components. Can you give an advise for which components…
Part Number: TIDA-010042 Other Parts Discussed in Thread: TIDA-00120
In both TIDA-010042 and TIDA-00120, Q1 is oriented with the body diode conducting in the direction of current flow. It seems then that Q1 is wholly ineffective as a switch, and merely…
Part Number: TIDA-010042
Can some one share clear documentation for starting the TIDA 010042. I flashed the program using ez-Fet lite. Now i want clear documention or suitable material to start the board for experiments. I want to use Electronic load…
Part Number: TIDA-010042 Other Parts Discussed in Thread: SM72442 We are currently looking for a MPPT solution to directly power a resistive load (2.7 Ohm, 1000 Watt max power rating at 48V) from two parallel-connected solar panels providing up to 48V.…
Part Number: TIDA-010042 Hi Team, seeking clarification. can the TIDA-010042 charge a battery while at the same time power a load? then In addition to that, is ir also capable of powering the load using the battery in case the solar is not generating enough…