Part Number: TIDA-010232 Hai,
We want to design a circuit similar to the TIDA-010232 for Insulation resistance measurement for our battery operated EV Vehicle.
From the reference design we will face an issue of continuous discharge through the HV Bus monitoring…
Part Number: TIDA-010232 Other Parts Discussed in Thread: TIDA-01513 , Hi, I was looking at the TIDA-010232 reference design and saw that it is proposed as a solution for EV charging stations, whereas TIDA-01513 is proposed as a monitoring device for EVs…
Part Number: TIDA-010232 Dear Team,
Do we have this reference design board can provide to customer for testing?
Can customer buy it from ti.com?
Many Thanks,
Jimmy
Part Number: TIDA-010232 Hi , I am trying to use the Insulation monitoring Device from your reference design TIDA-010232 , I see you have connected it with launch pad and provided some software to use , so why the connection with the board and launchpad…
Part Number: TIDA-010232 Other Parts Discussed in Thread: AMC3330 , TLV6001 Hi Ti,
I use Pspice to simulate reference design TIDA-010232 to calculate RisoP and RisoN, but answers are not correct.
Could you please give me a hand?
Please refer to the schematic…
Part Number: TPSI2140-Q1 Other Parts Discussed in Thread: TIDA-010232
Dear TI Team,
I'm currently reading the Design Guide: TIDA-010232 AFE for Insulation Monitoring in High-Voltage EV Charging and Solar Energy Reference Design. In this file, insulation…
Part Number: TPSI2140-Q1 Other Parts Discussed in Thread: TIDA-010232 , , TPSI2072-Q1 Hi,
Customer refer design Guide: TIDA-010232 to insulation Monitoring, they system voltage need 1500Vdc max, but the design is for 400Vdc system,
Do you have an idea…
Hi Seungmin,
Saleh Ahmad said: The AMC131M03 has an internal PGA. You can set the Gain to 128, which would make your full-scale input +-9.375mV. For +-30mA, a shunt value of ~0.31Ohms would be good (9.375mV / 30mA = 0.3125Ohm). I'm not sure what the power…
Part Number: TPSI2140-Q1 Other Parts Discussed in Thread: TIDA-01513 , TIDA-010232 Could you please share the details for the Simulation (spice model )for this TPSI2140-Q1. So it will helps us to simulate with all the extreme conditions.
Part Number: AMC3330-Q1 Other Parts Discussed in Thread: AMC3330 Hi all,
I have referred the insulation monitoring for DC load system with respect to chasis https://www.ti.com/tool/TIDA-010232
Our requirement is to measure the AC insulation system with…