Part Number: TIDA-020031 Hi team,
I want to know the Big Power Transformer P/N, But the BOM of T6 is Coupled Inductor (I't not correct!).like the circle in the photo!
Can you help me to find that right P/N of Power Transformer?
Thank you very much…
Part Number: UCC28950 Customer is referring to both TIDA-020031 and SLUA560D
They have some questions about how max Duty cycle is selected.
SLUA560D use 70% as the max duty cycle in equation (4),
In design, use a center-tap transformer, which leads to…
Hi,
Thank you very much for your answer. It has been very useful to me. I also want to ask what are the advantages and disadvantages of TIDA-020031's rectification method compared to PMP8740's rectification method?They used the same number of SR.…
Part Number: UCC28951 Hi,
RnD looks for DC-DC solution 5KW and 10KW, Vin: 800V / Vout: 28V.
Is UCC28951 suitable for 5KW and 10KW? Do you have any reference design for this application else TIDA-020031?
If it's not, could you kindly help to suggest suitable…
Other Parts Discussed in Thread: UCC28951-Q1 , UCC28951 Dear Team
We are developing DC-DC converter for trucks as per below specifications.
We Have studied the TI reference design TIDA-020031 which is closer to our project, major difference is operating…
Part Number: UCC28951-Q1 Other Parts Discussed in Thread: UCC28951 Hi,
I am designing a phase shifted full bridge circuit using the TIDA-020031 reference design, with an output voltage of 20V, a current of 150A, and a maximum power of 3000W.
The transformer…
Part Number: LM7480-Q1
Hi to all,
I'm designing an output safet switch similar to the one described in TIDA-020031 reference design, but I'm wondering if LM74801-Q1 could be used in a bidirectional DC-DC converter. Looking at data sheet I found this…
Dear Vikas,
In this case you may want to consider the TIDA reference design TIDA-01604 ( https://www.ti.com/tool/TIDA-01604), which is a 6.6KW totem pole PFC specific designed for onboard chargers (therefore uses automotive grade components). I believe…
Ray,
Thanks for reaching out here. For this EV charger design, do you know if they require AEC-Q100 qualified components here or are they ok with industrial grade (if it's an EV charger external to the vehicle I would assume Industrial grade is ok, but…