The link opens at my side. Quote from the post " HSM mode on CC1310 refers to 4mbps fixed datarate with 8FSK modulation. It is possible to achieve 1mbps datarate 2(G)FSK and upt0 1.5mbps 4(g)FSK (programmable datarate) on this device as well in the…
Part Number: CC113L Hi,
Our customer use CC113L, and the frequece need 915MHz. Now refer CC113LEM 868/915 MHz Reference Design.
The question is how to change to 915MHz? Which 2 discrete component and change to what value?
By changing 2 discrete component…
Hi,
The BALF-112X-02D3 was never released for the CC1120 from TI. There is no matched conjugate filter balun at 433 MHz for CC1120; only at 868/915 MHz.
The supported matched conjugate filter baluns (IPCs) are listed in Section 8 in the SWRA640 app note…
Part Number: CC1120 Hi,
I need to switch my product between 868MHz for Europe and 915MHz operation for the States. 868MHz works fine, 50ksps 2-GFSK, 32MHz xtal. FREQ2,1 settings are 0x6C, 0x80.
When I switch to 915MHz by changing FREQ2, 1 to 0x72, 0x60…
Part Number: CC1120EM-868-915-RD Other Parts Discussed in Thread: CC1120 hey,
Want to configure Evaluation module CC1120 using smartRF studio 7 but i am using another devlopement board is it possible to configure cc1120 with RFstudio 7?
In devloper's module…
If you are able to receive the same range with genfsk in one direction (collector to nodes) as in the other direction (nodes to collector) using SimpleLink LR this can be a solution depending on what your system spec. is requiring. On the node side, transmitting…
Other Parts Discussed in Thread: CC1120 , CC1101 Hello, we need to redesign one of our old receiver circuits for remote control applications (garage doors, etc). This works with 1000+ old transmitters in 868 MHz ASK mode. Any replacement must be downwards…
Good morning, sure I can provide some more info:
The aim is to get better than the old analog receiver, which is used till today. So I made a real life test with the analog receiver in parallel to the CC1120 DVK, both radiated. The data output of both…
Part Number: TIDC-SIGFOX-CC1120-CC1190-BP Hi,
I am evaluating Ti's Sun-1GHz CC1120-CC1190 boosterPack reference design for sigfox networks. I have modified the boards to make it operate at 868 MHz. So right now I am doing some performance testing with…
Part Number: CC1101 Other Parts Discussed in Thread: CC1310 Hello,
I am an intern here at Texas Instruments, and am working on a project within the BMC group. I am having to design and create a board that has multiple functions, one of which is to be able…