Part Number: TIDM-02006 Other Parts Discussed in Thread: ISO7820LL , TMDSFSIADAPEVM , ISO7763 Hi Team, Taking a cue from the TIDM-02006 design guide, our customer has these questions: - In daisy chain FSI, are digital isolators (example: ISO7820LL) like signal…
Part Number: TIDM-02006 Hi Team,
I found that many of our motor control SDK programs are in the form of links. What should I do if I want to create a different test version? Is there any easy way? (Because the file is in the form of link, no matter what…
Hi Paul,
Paul Reshetikhin said: Would it be possible to also use the TMS320F28P559SJ in conjunction with another TI processor to leverage the Instaspin-Motion motion profiling? If so can you offer a recommended solution for this?
InstaSPIN Motion can only…
Part Number: TIDM-02006 Hi there,
We have just start looking into reference design TIDM-02006 and have some questions regarding its manual (TIDUEV1):
1. Referring to figure 9, with FSI, what is the max. possible comm. frequency between position and speed…
Well using that device you have the option of EtherCAT. This is a high bandwidth lower latency link with automatic timestamping which would be beneficial for your application.
PM bus has been used in applications with similar requirements as yours.
FSI…
Part Number: TMS320F28388S Other Parts Discussed in Thread: C2000WARE , TIDM-02006 Hi expert,
F28388S has no CM4 core right? If we would like to use F28388S to do EtherCAT, the protocol will be running in CLA core? Are there any app notes for F28388S for…
Hi Sid,
Thank you for your response. I got feedback from the customer, please see below.
"I finished reading the article, I will try to read it several times so as not to miss anything. where can I find an example code that helps me to forward ethernet…
Part Number: TMS320F28388D Other Parts Discussed in Thread: TIDM-02006 , C2000WARE Hi,
Is there any way to use the fcl_f2838x_tmdxiddk_cpu1 example with CPU2 configuration?
Thank you
You can use any of the communications which are on both devices. SCI, SPI, CAN, FSI, etc.
If it has to be isolated consider how many lines are crossing the isolation boundary.
Look at your data throughput required and select one.
I recommend FSI, its…
For your query 1 on FSI networking and sync
FSI is a valuable IP that are being used in many multi-node applications. Refer to the following TI designs and app. notes that can add more light into the use case for FSI.
FSI Adapter Board User’s Guide…