Hi Jayakeerthana,
Jayakeerthana P said: Is there any reference design available for scaling resolver input signals to 3,3v to provide it to the AM263P2 processor?
As mentioned on AM263P4-Q1: Arm-based microcontrollers forum
Please refer to the reference…
Hi Shoji,
Since each board will drive a half bridge, you can use 3 of those boards. Please refer to this reference design here: https://www.ti.com/tool/TIDM-02014
Regards,
Akshat
Part Number: TIDA-01527 Other Parts Discussed in Thread: TIDM-02014 HI Team,
There's an issue from the customer need your help:
May I ask what method can be used to output the real-time angle of the motor rotor position in real time? In addition,…
Hey Faiz,
Thank you for the kind words regarding TI. We are happy to help you achieve your design goals!
Yes, a square wave would be a bit easier to realize, but it is important to recognize that this will still be challenging to realize.
It is…
Hi David,
Good to hear from you again!
The error of internal VREF contributes a significant amount of error to the ADC. This is seen in the fact that the INL is 1.2LSB with external reference, and -4/+9 LSB with internal.
More specifically, the…
The description, design files and technical details can be found here, https://www.ti.com/tool/TIDM-02014
You can purchase this kit directly through our partner, Wolfspeed, as we do use the Wolfspeed XM3 power modules.
We do have the following UCC5880INVERTEREVM…
Hello JM,
Thank you for reaching out!
IF you look at the recommended operating conditions of the UCC587x family of drivers, 15A is actually the listed output current, though this driver can deliver a much higher instantaneous current, which is why…