Other Parts Discussed in Thread: MSP430F4250 Hi I use the MSP430f4250
And I take readings from SDA16 channel 0 every 2 Seconds (I use basic Timer)
When the microcontroller take readings works on POWER MODE 0
the rest time the works on POWER MODE…
Hi,
I have implemented the code which is able to communicate with rtc DS3231M. I am able to read and write the data from DS3231M. I am using the i2c_if.c file using the function int I2C_IF_Write(unsigned char ucDevAddr, unsigned char *pucData, unsigned…
Part Number: MSP430I2021 Other Parts Discussed in Thread: TIDM-3OUTSMTSTRP , TIDM-TWOPHASEMETER-I2040 Hello,
I am working on a design that utilizes an MSP430I2021. In this design, an analog signal proportional to a temperature reading is connected…
John,
My code doesn't work. Actually I combined two codes (both are working) to have a single code, but the combined code doesn't work. I am working with ezdsPTMF28335 to a Ball and Beam Control system.
Code1:(Working)
#include "DSP2833x_Device…
Part Number: MSP430F6779A
Hi TI Support,
I suspect about connect capacitor with pin MCU of MSP430F6779A.
Which pin of the mcu if there is no connection to a capacitor? It will cause the mcu to not start-up.
Using 100-Pin PZ Package
Data…
Part Number: TIDM-MSP430AFE253SUBMETEREVM Other Parts Discussed in Thread: MSP430AFE253 , MSP430I2041 , EVM430-I2040S Hello,
I was reviewing the TI design of the single phase energy meter using built in AC/DC converter, and as per the schematic the…
Kanemaru
The LF02 and LF05 suffixes are to indicate Lead Free status. Functionally they are identical.
You asked about heatsinking information on the NDH package however the mechanical drawing you included is the NEB package.
For the NDH (Vertical…
Its a works in progress.
I have an FPGA model of TIDM-HV-1PH-DCAC tha t I have connected to a TMS320F28379D Launchpad via an interface card adapter.
I am following the Voltage Source Inverter Design Guide
Voltage_Source_Inverter_Design_Guide_tiduay6b…