Part Number: BEAGL-BONE-BLACK Tool/software: Hi,
I have connected ethernet cable to Beaglebone Black then power it on using USB cable. But, I can't open 192.168.7.2?
-kel
Part Number: DP83TG720S-Q1 Other Parts Discussed in Thread: DP83867E Tool/software: Hi Community,
I have a short question regarding my design for a SPE interface where I'm using the DP83TG720S-Q1.
The signal path is the following:
NVIDIA Jetson…
Part Number: TMS320F28027PTT
Hi, I want to design a schematic using TMS320F28062PZT and TMS320F28027PTT as master and slave respectively. I also want to have an ethernet port connected to slave. can you please help me out in designing the schematic…
Part Number: AM3358
Tool/software:
Hi everyone,
I am new to microprocessors, Linux and networking so I need your help for my project.
I have this device with an AM3358 processor that I would like to use as a DANP device. It has two ethernet ports…
Part Number: AM2634 Other Parts Discussed in Thread: DP83869 , DP83869EVM Tool/software: Hi All,
We have used AM2634 in custom PCB board which will have ethernet, UART and JTAG connectivity. We were able to get UART and JTAG working. But, we are facing…
Part Number: AM62A7 Tool/software: Hi TI forum,
We are developing a custom AM62A7-based board with ethernet. In our board, we are using the KSZ8775 switch chip from Microchip. The switch's port 5 is used for RGMII connection with AM62A7. Below is the…
Part Number: AM6421 Tool/software: Hi,
using AM6421 SOC and sdk ind_comms_sdk_am64x_09_02_00_15.
Protocol - Ethernet/IP
On AM6421 Board created first connection with below settings
1) Class Ids #define EI_APP_DIO_DEVICE_DIP_CLASS_ID 0x08 /*!<…
tamaru.kb said: Question 1. For peak current mode, is R50 removed and used?
R50 needs to be removed as stated in the guide.
tamaru.kb said: Question 2. Does the peak current mode require a smaller bandwidth consisting of R32 and C23? At 1kohm and…
Part Number: TDA2E Other Parts Discussed in Thread: TDA2 Tool/software: Dears,
Our project uses TDA2x and TC397 Ethernet direct connection, with TDA2x internal switch as shown in the screenshot.
My question is whether the connection between TDA itself…