Part Number: EVM430-F6736 Other Parts Discussed in Thread: TIDM-3PH-ENERGY5-ESD Dear Mr Erick,
This has reference to your slides shared in related thread.
Need help on couple of freq measurement related implementation in TIDM-3PH-ENERGY5-ESD_1.1 1…
Hey Cash, Thank you for info. i will try it and let you know if it worked. one mor question: like described in the docs attached, i had to do some modification on the board, which i did. and the problem is, the Transducers will be conneted to CH0_OUT…
Rana,
1. F28377S has 2 Flash banks, so OTA is possible. Strictly speaking, AUTOSAR FOTA on this device will require 3 Flash banks.
2. You have to set it up properly during production, and make it OTA ready.
3. You can start by referring to spracn0…
Ercan,
*Note that TIDM-1005 has been obsolete since 2021, so there is no longer any direct hosting or support of the reference design. However, I would be happy to help you out from my own understanding and knowledge of the solution.
You might be…
ames,
I ran the system overnight and what I see is Energy Consumption periodically returns to zero and starts counting up again. How can I debug this? I cannot sync IAR halt exactly when the energy values are reset.
MSP430i2041 on custom hardware;…
Part Number: C2000WARE
Tool/software:
This FAQ covers F28x MCUs. It will be updated in the near future to cover F29x MCUs.
7587.LFU_ASM_2025_F28x_Public.pptx
Hi Paul,
Paul Reshetikhin said: Would it be possible to also use the TMS320F28P559SJ in conjunction with another TI processor to leverage the Instaspin-Motion motion profiling? If so can you offer a recommended solution for this?
InstaSPIN Motion…
Part Number: TM4C129ENCPDT Other Parts Discussed in Thread: TIDM-TM4C129POEAUDIO , , TPA3111D1 , OPA322 For our NVR project we need to make two separate Audio Boxes that will be connected with NVR over ethernet. This Box should be able to provide two…
Hello Satish,
satish sharma13 said: I need msp430f67791A sample code and is this contorller suitable to measure THD..
Are you using the MSP430F67791A or MSP430F67641A? Both can be used to calculate THD, but we only offer a F6779A-based TI reference…
Part Number: MSP432E401Y I'm currently designing a microcontroller board with MSP432E401Y which uses EPI Host bus muxed mode for interfacing with 3 devices(SRAM, Parallel Flash and FPGA)
To segregate the address and data line, should i add a D-latch…