Part Number: TIDM-02014 Tool/software: Dear all, thanks for reading
I would like to know if there's a chance to acquire the design files created for the reference designs.
Assuming there's a mechanism to get them I would like to discuss such a possibility…
Part Number: AM6422 Tool/software: Hi Ti Team,
I have built the mcu app (ipc_rpmsg_echo_linux) for r5fss0-0_freertos based on the sdk 9.02.
It can start from the linux side, but after running, stop the remote core will get timeout.
Here is the log for…
Part Number: TIDM-02012 Tool/software: Are there any updates regarding dynamic vibration compensation algorithm on the Mathworks model like disucussed here: ? e2e.ti.com/.../tidm-02012-model-files---dynamic-vibration-compensation
Part Number: DP83869HM Tool/software: I want to design one board using media convertor concept and it will convert RGMII to 1000Base-X(copper to fiber mode) without using MAC interface.
I strucked in design part of this and queries are:-
1. I dont want…
Part Number: UCC28600 Other Parts Discussed in Thread: UCG28826
Tool/software:
Hello,
I am currently working on a project to design a GaN-based Power Factor Correction (PFC) and Quasi-Resonant (QR) controller. My specifications include an output power…
Hello Charles, The XOR that the FAQ and the TRM both refer to, just describes how the device loads up the programmed OTP values. This BQ76952 OTP FAQ answers what are they key things to be aware for OTP programming with our device. As mentioned previously…
Part Number: UCC27282 Tool/software: Hi Team,
Do we have recommended DC to AC solution for driving PDLC?
Input voltage is 5VDC supplied from adapter. Output requirement: AC output voltage ~40VAC, output power ~10W.
Could you please check whether the…
Part Number: PMP23146
Tool/software:
Hello all, I came across PMP23146 which is a Auxiliary Supply Reference Design for Server PSU. However, as per the Open Compute specifications for M-CRPS, Load sharing (using droop control) is an integral requirements…
Ashik,
This is a very generic question. We have PWM examples, which you could then use to control each half bridge.
I think a better route would be for you to look through our digital power reference designs: https://dev.ti.com/tirex/explore/node?node…
Part Number: TIDM-SMARTMETERBOARD3 Hi all,
Currently I am working on communicating two can controllers. One controller is connected Arduino board and other controller connected to teensy board. Individually both can controllers are working like send…