Part Number: INA240 Other Parts Discussed in Thread: TL081 , TMCS1100 , TEST , TLV2461
8.3.1.2 Input Signal Bandwidth
The INA240 input signal, which represents the current being measured, is accurately measured with minimal disturbance from large ΔV/Δt…
Part Number: EK-TM4C1294XL Other Parts Discussed in Thread: TEST , TL081 , LM741 Single ended analog input signal 1.65v threshold has poor digital granularity for magnitude changes > +/-100mV relative mid VREFP.
How can ADC single ended sensitivity be…
thank your reply.
I change lm324 to tl081. it is working without kik off voltage @ t=0. but i face another issue when design sine generator & simulate both at same time , sine is not coming). when simulate separately it is working. how rectify this…
Bell,
If "OPA" can mean op-amps from other prefixes other than OPA series, then these are high voltage op amps with high VID tolerance (and low cost).
TS321, LM358, LM324 family of devices.
TL031, TL061, TL071, TL081 where 1 = {1,2,4}
RC455…
Hello Kai
Some progress...
I removed the components from my breadboard and used them to rebuild a circuit on a new breadboard, according to your guidelines. A photo is below (op amps left to right: U1, U2, U3; blue wires are ground grid). I kept the same…
Part Number: OPA659 Other Parts Discussed in Thread: TL081 Hello
I have studied some papers. I found some useful topics and would like to share it below. But I couldn't manage this technique with OPA659 unity gain! could you please help me?
the…
Other Parts Discussed in Thread: TL081 We are using 3 Power Mosfets IXTX40P50P in parallel and driving them through an Op amp TL081 in a current source of 0-5 A. The sources are tied and are supplied with 25 V through a sense resistor of 1 Ohm. The gate…
Other Parts Discussed in Thread: LM6171 , TL081 , OPA322
Greetings everyone,
I am going through the TIDU765 design (John Caldwell) in an attempt to grasp the details of the Eletret microphone.
This article is great work being clear and precise. However,…
First your peak detector will require high currents during transients. If output of TL081 is near 13V then peak current out is 13V/10 ohm or 1.3A thorugh the 100nF capacitor. Max R-C for load on TL081 for stability would be 100 ohm and 10nF but this is…
Other Parts Discussed in Thread: TL081 , OPA827 , TINA-TI Hi everybody,
I would like to make a current source with current output 500 uA with frequency range from 50 kHz to 200 kHz. I would like to use this source for bio-electrical analysis. So, the R_LOAD…