Part Number: TL1431-SP Other Parts Discussed in Thread: TL1431 , , TL431 Question about using the TL1431 as a delay circuit in the comparator mode. This would be open loop mode with a resistor to the ref pin and capacitor to ground. The ref input through…
Part Number: TL1431-SP Hi team,
My customer wants to know if the TL1431-SP has a metal lid. If it does, they want to check if the metal lid is internally grounded, or provides a pad for floating, or is floating.
Can you please help and provide if they…
Part Number: TL1431-SP I am currenlty building an FMECA document and we are using the TL1431-SP part from TI. Is there any information regarding the component level failure mechanisms that could help me fill the information for this part? Are there any specific…
Part Number: TL1431-SP Hello,
I'm using 5962R9962001VHA (Flatpack package) IC. However, the datasheet is confusing about NC pin connections. 1-) Do you have any SMD datasheet?
In page one, it is written that "NC-No Internal Connection". However, in…
Part Number: TL1431-SP Other Parts Discussed in Thread: TL1431 , TL431 , I will be using SMD # 5962R9962001VHA. My application is the following:
Power Supply input 3.3V (+/-4% tolerance), TL1431 configured for 3V output.
The TL431.xlsx tool calculator suggest…
Part Number: TL1431-SP Could you let me know the package information as follows?
P/N: 5962-9962001VPA
・Package material/ base plating /plating (ex. Ceramic(Alumina)/Ni/Au
・Lid material/ base plating /plating (ex. Covar/Ni/Au
・Package cavity wall thickness…
Part Number: TL1431-SP Hello,
Can you confirm that the NC pins on this device are truly not connected to the die?
We cannot leave these pins floating. Is there a recommendation for this?
Can we connect them directly to GND? Would we need a resistor to…