Hi Sudheer,
Q1. Step 1: Ping eth0 (via J35) successfully. Step 2: Ping eth1 (through quad port) successfully. Step 3: Ping eth0 (via J35) failed. Do you mean that this phenomenon is due to the limitations of the EVM network topology?
Q2 Please refer to the…
Part Number: TL2575HV-05-Q1 I want to know efficiency calculation for this part number TL2575HV-05-Q1 with formula.
Vin = 54v and Iload = 500mA
Please reply me as soon as possibile.
Part Number: DLPC120-Q1 Tool/software: Hi,During the test of our DLPC120+DLP3030 system, RE did not meet the requirements (AV value of about 76MHz exceeded 3dB). After investigation, it was caused by the clock at the DMD interface. We have done shielding…
haitang wang said: we add the user muticast address but not show on the ALE table,you can try add the new muticast address 。Thx
Hi Haitang
verified on SDK9.1 Jacinto7,
multicast frame can be received on A72 Linux
see following debug log:
-------…
Part Number: LM5069 Other Parts Discussed in Thread: CSD19532KTT
Tool/software:
Abstract
It was noticed that bad connection on the power supply cable can cause some sort of ‘fault loop’ on the LM5069 circuit, from which it usually cannot automatically…
Part Number: TMS570LC4357 Tool/software: Hello ,
Q1 -) i coundt find any document that shows the clock source of the ECAP module on the TMS570LC4357 mcu ? It shown as SYSCLK in the trm Figure 33-6. Counter and Synchronization Block , but what is SYSCLK…
Part Number: TPS2HCS10-Q1 Tool/software: Hi team,
My customer is considering to use TPS2HCS10-Q1 in a ZCU project. They are evaluating the thermal performance of the device. In their application, only 1 channel of TPS2HCS10-Q1 is used and the current…
Part Number: DS90UB927Q-Q1 Tool/software:
i am use 927 and 928 to send lvds single . i use video source pixclk is 26.2MHz . But in anlog launchPAD pixclk is 33-36MHz instability. 2 picture is use PG Timing Source = internal and interal w/ext.clock.…
Part Number: TPS6594-Q1 Other Parts Discussed in Thread: TDA4VL Tool/software: Hello,
The PMIC we used is TPS6594133ARWERQ1, SoC is TDA4AL or TDA4VL, and the power supply scheme we use is the J784S4 PDN-3F.
At present, we find that as long as SOC_RAIL_TRIG…