Part Number: TL5001 Other Parts Discussed in Thread: LM3478 Hello,
I have been looking for a device to control a PWM as a controller and the TL5001 seems to be perfect for my needs.
However, pulling a datasheet with a 1994 release date (and old TI format…
Part Number: TL5001 Hello,
I want to replace MAX635/MAX626 by a TL5001, as I have seen that this controller can be used as inverting controller. Is there anywhere schematic example to obtain -5V from a 5V input ?
If I remember, I have seen a long time…
Part Number: TL5001 Hi Team,
The customer uses TL 5001 as a PWM waveform generator. He wants to adjust the operating frequency to 20 kHz. In the data sheet, the recommended value of the frequency setting resistor Rt is 15 kΩ to 250 kΩ, and the recommended…
Part Number: TL5001 I am working on a design that will use the TL5001 . It is a DC-DC high Vout flyback converter(Isolated DC/DC).
Issue:
1.I use 100K resistance between RT & GND, System work oscillator frequency is 22K when on load is 3W, 100K at no-load…
Part Number: TL5001 Other Parts Discussed in Thread: TINA-TI , TPS40210 , LM3481 Tool/software: TINA-TI or Spice Models Hi team
IC model (IBIS, Spice, S-parameter) data is required.
I checked it on the homepage but it is hard to find.
If you have, please…
Part Number: TL5001 Other Parts Discussed in Thread: LM3478 , LM3481 Dear sir/madam,
I am currently using TL5001 for boost converter design. The input is 5V, output is 12V. The power level is around 12 W.
I use N-mos IRF8707 for the main switch. The inductor…
Other Parts Discussed in Thread: TL5001 , TPS40200 , TL494 , UCC35701 , SG2524 We are designing a PWM voltage mode control circuit for a buck converter using TL5001. The design requires a frequency of 10 KHz(KW power IGBT application).
There is a discrepan…
Other Parts Discussed in Thread: TL5001 , TPS40200 Dear TI
I'm looking for means to simulate my DC-DC circuit, using the TL5001 . On the product page there in no linked PSpice or TINA model.
I would like to know;
A: Does a simulation or web-design model…
Other Parts Discussed in Thread: TL5001 Hello, I have a question about the Error amplifier of the TL5001. In the detailed description of the error amplifier the datasheet say's:
The error-amplifier output is brought out as COMP for use in compensating…