Other Parts Discussed in Thread: TL5001 , TPS40200 Dear TI
I'm looking for means to simulate my DC-DC circuit, using the TL5001 . On the product page there in no linked PSpice or TINA model.
I would like to know;
A: Does a simulation or web-design model…
Other Parts Discussed in Thread: TL5001 Hello, I have a question about the Error amplifier of the TL5001. In the detailed description of the error amplifier the datasheet say's:
The error-amplifier output is brought out as COMP for use in compensating…
Other Parts Discussed in Thread: TL5001 Hello,
I am working on a design that will use the TL5001 . It is a DC-DC high Vout flyback converter. Unfortunately, the datasheet does not specify if a flyback configuration is inherently possible with this chip hence…
Other Parts Discussed in Thread: TL5001 Hello,
I am working on a design that will use the TL5001 . It is a DC-DC high Vout flyback converter. Unfortunately, the datasheet does not specify if a flyback configuration is inherently possible with this chip hence…
Other Parts Discussed in Thread: TL5001 Hello, I'd like to use the pdip TL5001 buck converter with over current protection on load current. But how? Another design to create the constant current source for a lead acid charger with max Vout limit. Also…
Other Parts Discussed in Thread: TL5001 , TPS54672 I have a TL5001 which i would like to use as a variable output regulator (this is a "tracking pre-regulator" for a linear PSU. I want the output to be just a few volts above the final Vout to minimize dissipation…
Bad news, Youhao.
I have wired a test and TL5001 doesn't start.
Green is GND, white is +15V and I expect between black and green around -100V.
I have simplified my test and I have removed D3, R9, Q3 and Q4. Now, I have put a 15V power supply between…
Other Parts Discussed in Thread: TL5001 , LM3524D Hi,
I'm looking to use a TL5001 as an analog-voltage-to-pwm generator. I saw an app note AN292 that explained how to do it with another chip, but I would like to get it to work with the TL5001, due to its…
I use the circuit same as a application note. But modify the gate drive with the high side gate drive circuit. It's not have a voltage at output like a voltage can't across SD of mosfet. by at the pass I use this circuit with open loop with the external…