Part Number: TL7715A Other Parts Discussed in Thread: TPS3700 Tool/software: Hi,
i'm looking to use this IC ,i had a few questions
if i was to detect voltage below 13V
how do i configure the circuit?
can i use this circuit with an active low…
Part Number: TL7715A Hello Team, I am using the voltage supervisor IC TL7715ACD in one of our projects," I want to monitor +15V and -15V. Attached is the schematic of the same. Please let us know if there are any mistakes. Also, what is the role of the…
Other Parts Discussed in Thread: TL7715A , TPS3700 , TPS3701 Hello all,
I have an application where I want to use the TL7715A and was hoping for some guidance.
The application is automotive, I want to monitor and take action based on the charging…
Part Number: TL7705B Other Parts Discussed in Thread: TL7715A , , TPS3700 , TPS3702 , TPS3701 Hi,
We use the TL7705B to monitor a couple of 5V rails and would like to adapt it to monitor a 15V rail (the TL7715A doesn't have the needed temp range for…
Other Parts Discussed in Thread: TL7705A On attached TL7705A datasheet P2, writing about Internal resister of SENSE-Pin.
TL7705ACP.pdf
I substituted and calculated Vref:2.48V~2.58V (and TL7705's R1,R2).
As a result, VIT-:4.41V~4.59V.
It's difference…