Part Number: TLC3704 Tool/software: 1. The schematic diagram is as follows:
2, Adopt TLC3704, input pwm1_A, blue waveform, output PWM1_TOP, red waveform; 3, when the power supply voltage is 5V: input frequency 7K 5V PWM square wave, the output is normal…
Part Number: TLC3704 Other Parts Discussed in Thread: TLC139 Hello. We were told 5962-9096901M2A (TLC3704MFKB) was going obsolete and the recommended alternative is TLC3704QDRQ1.
While the output type and parameters all match very close, TLC3704QDRQ1…
Part Number: TLC3704 Other Parts Discussed in Thread: LM311 , LM6511 , LM2903
Hi,
Can TLC3704IPWR be used in dual power supply configuration of +/- 3.3V or +/-5.0V
As VOL = is mentioned as 400mV max and also application circuits or test circuit…
Part Number: TLC3704 Hi team,
My customer need the maximum junction temperature for TLC3704IPWR for a thermal analysis.
but I didn't find this info in the datasheet.
Part Number: TLC3704 Other Parts Discussed in Thread: TLV3704 Hi Team,
Customer is using comparator TLC3704 in one of the design, please see below query from component point of view:
TLC3704 is powered up by using +/-3.3V. And As per datasheet…
Part Number: TLC3704-Q1 We are using TLC3704QDRG4Q1 in our electric control module and have problem with slow response time. For some of the parts we measure in our eol test much longer delay, 10´s of us. The parts are marked 08AJS4M
In our testing…
Chris
We have not received a new post in a while so I am going to close this thread. If you have additional questions, feel free to respond to this thread again or open a new thread.
thanks
Chuck
Part Number: TLC3704-Q1 Other Parts Discussed in Thread: LM339 , LM393 , LM2901 , TLV7011 Hello,
Background
I have a "digital" signal that I need to monitor on a 5V microcontroller input pin. The signal has a value of ~12V for OFF and ~60V for ON…
Part Number: CD4504B Other Parts Discussed in Thread: UCC37324 , UCC27516 , TLC3704
Hello
I am looking for a Low to High ( 3.3 V to 15 V ) Translator with at least 10 mA Source & Sink
capability for Interface between our DSP and IGBT Drivers.
…