Other Parts Discussed in Thread: TLC5540 Hi, I am using TI TLC5540 ADC in one of my application. I have set REFT as 3.2V ( using external resistor) and REFB as 0V as per the design requirement. The input signal specifications are 2.9Vpp (-1dBFS from the…
Hi,
We are using TL5540i ADC in our application. We need IBIS model for signal integrity analysis. Request you to provide the same if it is available.
Thanks,
Srilakshmi
Other Parts Discussed in Thread: TLC5540 hello. I am for using the TLC5540. The data sheet says that the minimum rate of conversion is 5MHz. Does this mean that lower can not convert signals to 5MHz?. My idea is to convert signals from about 100Hz to …
Other Parts Discussed in Thread: TLC5540 Hi,
We are using the TLC5540 chip on our board interfaced to a Virtex6 FPGA (Schematic attached).
We are using it for sampling an input video signal fed from a Function Generator (with 50ohm output impedance) at…
Other Parts Discussed in Thread: TLC5540 , TXB0108 From the datasheet of the TLC5540. I have some questions i can not sure. 1.If i want the chip of TLC5540 can operate with Vreft - Vrefb = 5 V ,i connect the pins "REFBS" and "REFB" to the GND, and connect…
Other Parts Discussed in Thread: TLC5540 Hi all,
I'm going to use TLC5540 with PIC18F4550 microcontroller.
Do I need 74AC573 IC when interfacing microcontroller and ADC .
(I'm referring the application note "Interfacing the TLC5540 Analog…
Other Parts Discussed in Thread: TLC5540 Hi all,
I don't know whether this is the place to post my post..
Any way i ll tel the problem.
i'm going to make a DAQ with help of TLC5540 (ADC) and PIC18F4550.
i have read the "Interfacing the TLC5540…
Other Parts Discussed in Thread: TLC5540 Hi all,
I have been using TLC5540IPW for analog input range of 0 to 2.5V with internal bias option in multiple projects.
but now i want to use it for 0 to 5V range, but could not.
I found in datasheet that by connecting…
Other Parts Discussed in Thread: TLC5540 I was wondering if there is any documentation on the transistor types used in some of the high-speed ADCs. I'm interested in low-temperature operation for research. I'm interested in a large range of ADCs (50 MSPS…