Part Number: TLC59116 At page 1 of datasheet i see "5.5-V Tolerant Inputs", but at page 7 i see AMR for inputs is Vcc+0.4V.
Can i use TLC59116 with 3.3V supply and 5V bus voltages ?
Part Number: TLC59116 Other Parts Discussed in Thread: TLC5940 ,
Hi Experts,
Would like to ask your confirmation if the part TLC5940 can be considered drop-in replacement for TLC59116. Any changes to need be adjusted here?
Please help me confirm their d…
Part Number: TLC59116 Other Parts Discussed in Thread: LP5562 , Hi,
I find a use information for lp5562: https://git.kernel.org/pub/scm/linux/kernel/git/torvalds/linux.git/tree/Documentation/leds/leds-lp5562.rst
Is there a similar doc/guide for TLC59116…
Part Number: TLC59116-Q1
Hi,
I want to use TLC59116-Q1 led driver but I'm not sure about the current. I will use 16 LEDs and 50mA each. Can i drive The scale available in the datasheet is as follows.
But given examples are maximum 37mA.
My supply…
Part Number: TLC59116-Q1 Hi,
I want to use TLC59116-Q1 led driver but I'm not sure about the current. I will use 16 LEDs and 50mA each. Can i drive The scale available in the datasheet is as follows.
But given examples are maximum 37mA.
My supply…
Part Number: TLC59116 Dear Sir/Ms.
The function of Open-circuit detection mentioned in 9.3.1 is described in this paragraph. For open-circuit error detection, a channel must be on and the PWM must be off. But without pwm, there will be no Iout. Iout …
Part Number: TLC59116 Other Parts Discussed in Thread: TLC5940 , TLC59283 Hi, support team
My customer has the questions as follow:
Is there alternate part for TLC59116IRHBR?
Thanks so much.
Best regards, Yuki
Part Number: TLC59116 Dear Support team,
The supply voltage Vcc range for TLC59116 is defined as 3V~5.5V in the datasheet.
The other hand, the supply voltage Vo for LEDs is 17V as maximum.
So, TLC59116 allows different power supply Vo for LEDs from Vcc…
Part Number: TLC59116 Hi team!
Currently, using the “F” version part (TLC59116FIRHBR) which does not have the R-ext feature, we have left the R-ext pin floating since it's NC.
If we were to switch to the “non-F” (TLC59116IRHBR) version…