Part Number: TLC59116-Q1
Hi all,
Can you tell me the questions below?
Is it possible for this device to drive load with only GRPPWM or GRPFREQ register? If PWM register is 255 (max), will duty be 100% like the figure below?
If answer to the question…
Part Number: TLC59116-Q1 Other Parts Discussed in Thread: TLC59116 Dear all.
is there a way to increase the power on reset time?
Our customer is looking for 1us capable automotive device.
Thanks.
Part Number: TLC59116-Q1 I would like to connect a relay to 2 spare outputs in parallel. The relay voltage is the V+ voltage, 1 V drop accepted and the relay current is below the set current.
Freeheel diode is added as normal.
Is this possible ?
Part Number: TLC59116-Q1 Other Parts Discussed in Thread: TIDA-01500 , TIDA-01184 Hi,
Customer has the issue in EMI test on CHMSL lighting based on TLC59116-Q1.
Customer will compare the layout and schematic between the application and reference design…
Part Number: TLC59116-Q1 Hi,
In below condition, after ESD, TLC59116-Q1 doesn't operate as I2C command.
It's 2m I2C cable and pull up resistance is 910Ohm.
After ESD, TLC59116-Q1 output turns off and doesn't turn on with I2C command but confirmed…
Part Number: TLC59116-Q1 Other Parts Discussed in Thread: TLC59116 , Hi Team,
I currently use the TLC59116 for RGB management and I want to use it to manage one power LED (white or IR).
I see in the TLC59116-Q1 datasheet (page 31) that it is possible to…
Part Number: TLC59116-Q1 Dear TI Experts,
Now I am using TLC116-Q1 to drive 3 RGB, but I found green led is not as bright as red and blue led~
The current is about 20mA, I change REXT resistance from 720Ω to 360Ω, but led brightness is dar…