Part Number: TLC5941 Other Parts Discussed in Thread: TLC5940 Hi,
my customer is using TLC5941, but they find that sometimes 80mA is not enough for the system, they wonder if we have any device that can support
16 channel and higher current?
Or the same…
Part Number: TLC5941-Q1 Hi TI expert
we are developing an application where we want to vary the intensity of LEDs using tlc5941-q1, we are using the Imax current as 30ma.we are loading DC values as 63 since we want to drive complete 30ma current for each…
Part Number: TLC5941 Hi
Please help to check SCH, is there any problem?
The product is always damaged by 1% and the cause cannot be found
The maximum current used for each channel is 26mA,
thanks! SCH-WM_LOGO_20181010.pdf
Part Number: TLC5941-Q1 Other Parts Discussed in Thread: TLC5941 Hi Sir.,
my customer uses 10 TLC5941 to drive 160 LEDs for backlight. They use PWM mode with 6MHz GSCLK. below is the waveform. it looks correct for me.
They drive all LED in the same PWM…
Part Number: TLC5941 In the datasheet we have the figure of OUTPUT CURRENT vs OUTPUT VOLTAGE.
My customer configure OUT0 current to be 60mA, and OUT0 is connected to an LED, according to the plot, as long as the voltage of OUT0 is higher than 0.7V, the…
Part Number: TLC5941-Q1 Hello,
I have an application where there is not GPIO resources to monitor XERR but we need LED Open Detection. The plan is to periodically read out SID to see if there is an error in the SID register.
My question is what is the…
Part Number: TLC5941TLC5941:A total of 16 outputs ,I only used 15 outputs.I have added an external pull-up resistor in this XERR pin .But XERR is always output low. Then I am tryiing setting the XLAT pin. When XLAT is High ,XERR is always output High…
Part Number: TLC5941 Hi team,
My customer wants to clarify max output current variation of TLC5941 including errors introduced by load and line regulations.
1. Do you have any data for the max output current variation? I'm asking this questions becaus…
Part Number: TLC5941-Q1 Other Parts Discussed in Thread: TLC5941 , , TLC6C5724-Q1 Does TLC5941 support Auto_Repeat Mode?
As spec. say, we need to input 4096 GSCLKs in one period.
If we can't input fix GSCLK count, could we just input continuous GSCLK?…