Part Number: TLC5943 I have LED outputs where return path is shared (VIS led has IR led as return and vice versa)
Since the TLC5943 acts as a current sink and I will ONLY use either VIS or IR LED at once (not simultaneously)
Is the circuit below correct…
Part Number: TLC5943 I was wondering if the output of TLC5943 is constant current (can the part be run at 100% duty cycle with no modulation at output assuming that blank never goes low and GSCLK is 65535)
Part Number: TLC5943 Hi sir,
I am looking for the the junction to ambient thermal resistance RθJA value in C/W and the junction to case thermal resistance RθJC value in C/W. Can you share it to me?
Thanks.
Part Number: TLC5943 Hello,
For the grayscale (GS) data in TLC5943, how frequently can we write it in application? For example, change the GS value every 5 seconds? Will this operation damage the device?
The grayscale control clock (GSclk) has a frequency…
Part Number: TLC5943 1. The output data of TLC5943 Sout confirmed that TLC5943 had data misinterpretation problem. The writing value of BC: EF will be misinterpreted as DE.
EF: 1110 1111 DE: 1101 1110 (just moved one place to the left)
(confirmation of…
Part Number: TLC5943 Hi dear supporting team,
my customer use SN47LVC1G3157 for the GSCLK switching for TLC5943, the sch is as attached below: sn47lvc1G3157 ON-State Resistance:6ohm(TYP)Switch Capacitance:17.4pF (TYP),could you help confirm from osc …
Part Number: TLC5943 Our design uses two daisy-chained TLC5943 drivers. We want to enable Auto Display Repeat Function as shown in page 20 of the data sheet (SBVS101 - December 2007).
The microcontroller shifts in Brightness control data 0xFF, so bit…
Part Number: TLC5943 We have three TLC5943 driver chips daisy chained in our application.
We are latching data into the driver chips using Auto Refresh Data Function Timing 3 as shown in Figure 27 of the TLC5943 data sheet. So we clock in 3 x 256 bits…
Part Number: TLC5943 Team,
After erasing the micro-controller driving the TLC5943 LED driver and having a pull-up on the BLANK input signal, some of the output channels are still ON. Looking on the data sheet: Does need GS data to be greater than 0300h…
Part Number: TLC5943 Other Parts Discussed in Thread: TPS54200 hi
I have tlc5943 that I want to use for high current led .
this device can take 50mA.
can I use MOSFET to have more current capability?
like connect the gate of MOSFET to the output of tlc5943…