Part Number: TLC5943 Other Parts Discussed in Thread: TLC5940 I would like to confirm if the TLC5943 has initial reset requirements for the first serial data write.
The TLC5940 has a requirement for first write of DC data after power needs to have extra…
Part Number: LP5891 Other Parts Discussed in Thread: , TLC6948 , TLC6946 , TLC6984 , LP5890 , TLC6983 , TLC5943 , TLC5946 , TLC5948A , TLC5940 , TLC59401 , TLC5929 Hi,
Can the LP5891EVM be connected to external LED display(chips)?
Best Regards,
Yuji
Other Parts Discussed in Thread: TLC5943 Hello folks,
I'm using an Arduino to bit bang to the TLC5943 but I'm not having much luck. Here is my simple bit bang code:
#define BRIGHTNESS_CONTROL_BITS 8
#define GRAYSCALE_CONTROL_BITS 16
#define NUM_CHANNELS_PER_TLC…
Other Parts Discussed in Thread: TLC5943 , TLC5940 Hello,
I have a problem to control Tlc5943.
I used tlc5940 but i decide for tlc5943 for the 16 bit controller.
Can you help me?
Thanks.
Hello Picca-san,
It's no problem for driveability of TLC5951 between IC to IC if SCK can keep a timing on data sheet.
But SCK timing is depend on controller driveability , PCB layout or line capacitor on PCB board whether it need buffer or not for connect…
Other Parts Discussed in Thread: TLC5943 Hi All,
I'm using the TLC5943 in a multi-channel rgb module - 6 drivers for 2 channels of 4:1 scan rgb leds.
The Vled is 12V with voltage dropping series resistors inline with each led column. 5V for Vcc. …
Other Parts Discussed in Thread: TLC5943 Hi,
I'm using a TLC5943 to drive 5 x RGB LEDs in a new design (so it uses 15 of the 16 channels).
The peak current is set to 5mA/LED, and each channel only has a single LED attached, so the LED supply is…
Other Parts Discussed in Thread: TLC5943 you can change the program that starts when you turn the plate tlc5943evm-274? is written to the eeprom instead of the 16 rotating colors such as blue green red or any other modified by the user?
thanks
2 plates can be connected via rs232 tlc5943evm jtag or through the union of the 2 plates through TP10 TP11 pins etc or otherwise? because it can not connect via USB to a computer and control it with the same program in parallel there any way to control…