Part Number: TLC5951 Other Parts Discussed in Thread: TLC6C5724-Q1 , Dear team,
My customer was using TLC6C5724-Q1 but due to supply issue, they need to use some TLC5951 in the same socket. Those two devices can be P2P replaced considering the DCSIN, DCSOUT…
Part Number: TLC5951 Dear team,
In TLC5951 datasheet, it says Hold time tH0 is GSSIN → GSSCK↑, however in figure 1, it shows that tH is Clock fall to data fall, or clock rise to data rise, data is always behind clock for tH duration, this is a…
Part Number: TLC5951 Other Parts Discussed in Thread: TLC5947 , TLC59581 , TLC5948 , TLC5955 , TLC5957 , TLC5958 , TLC59582 , TLC59731 I am working on building a solution for controlling a few hundred RGB LED Pixels using only a SPI port (data out, data in,…
Part Number: TLC5951 Hello,
I am using a single 5951 to control 8 RGB leds.
ISSUE:
As GS values (for all LEDs) are raised from 0 to 4095, the LEDs brightness rises from zero to full on (100% duty cycle) every 256 steps (not 4096 as expected). This repeats…
Part Number: TLC5951 Dear all,
I would like to ask questions about TLC5951.
Our customer try to control only the input from GSSCK and GSSIN without input from DCSCK and DCSIN,
I would like to ask the following questions.
1.There is no example of using…
Part Number: TLC5951
Hi,
I am working on a schematic layout of TCL5951 on Altium and I have a question:
I was wondering what the values of the Resistors and Capacitors are on Figure 7. HPA477A Schematic 4 I looked at Table 2. HPA477A Bill of Materials…
Part Number: TLC5951 Hi,
I'm trying to use TLC5951 with AMPMAFB-33.0000 MEMS oscillator for Grayscale PWM clock signals, connected to GSCKR/G/B in parallel. As soon as the oscillator is connected to the TLC's pins, the clock signal breaks down, recovering…